DM3730 DVSDK,linux-2.6.37支持yaffs2后,挂载nand flash上的驱动后出来如下错误,标红部分为关键错误点,编译选项Kernel Feature里面的
-*- Use the ARM EABI to compile the kernel
[*] Allow old ABI binaries to run with this kernel (EXPERIMENTAL)
Texas Instruments X-Loader 1.5.0 (Oct 26 2012 - 14:33:47)
OMAP36XX/37XX-GP ES2.1
Loading u-boot.bin from nand
U-Boot 2009.11-svn37 (Oct 24 2012 - 16:38:26)
OMAP34xx/35xx-GP ES2.1, CPU-OPP2 L3-165MHz
OMAP3 da_b3730 + LPDDR/NAND
I2C: ready
DRAM: 512 MB
NAND: 512 MiB
In: serial
Out: serial
Err: serial
Ethernet MAC address: 02:2f:0c:02:c0:2b
Die ID #60ae00229e3800000168682f0c02c02b
Net: smc911x-0
Warning: smc911x-0 MAC addresses don't match:
Address in SROM is ff:ff:ff:ff:ff:ff
Address in environment is 02:2f:0c:02:c0:2b
Hit any key to stop autoboot: 0
No MMC card found
Booting from nand ...
NAND read: device 0 offset 0x280000, size 0x400000
4194304 bytes read: OK
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-2.6.37-svn41
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3323416 Bytes = 3.2 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 2.6.37-svn41 (ss@ubuntu10) (gcc version 4.3.3 (GCC) ) #1 Thu Nov 15 14:54:50 CST 2012
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: OMAP3 EVM
[ 0.000000] Reserving 12582912 bytes SDRAM for VRAM
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] OMAP3630 ES1.2 (l2cache iva sgx neon isp 192mhz_clk )
[ 0.000000] SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x10000
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 126976
[ 0.000000] Kernel command line: console=ttyO0,115200n8 vram=12M omapfb.mode=dvi:1024x768MR-16@60 omapfb.video_mode=dvi:1024x768MR-16@60 omapdss.def_disp=dvi omap-dss.def_disp=dvi rootfstype=yaffs2 root=/dev/mtdblock4 rw init=/bin/sh mpurate=600 boardmodel=EVM35X-B3-1880-LUNC0
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 500MB = 500MB total
[ 0.000000] Memory: 494668k/494668k available, 29620k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
[ 0.000000] vmalloc : 0xe0800000 - 0xf8000000 ( 376 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .init : 0xc0008000 - 0xc003f000 ( 220 kB)
[ 0.000000] .text : 0xc003f000 - 0xc0635b1c (6107 kB)
[ 0.000000] .data : 0xc0636000 - 0xc07f8660 (1802 kB)
[ 0.000000] NR_IRQS:409
[ 0.000000] Clocking rate (Crystal/Core/MPU): 26.0/400/600 MHz
[ 0.000000] omap_hwmod: i2c1: softreset failed (waited 10000 usec)
[ 0.000000] omap_hwmod: i2c2: softreset failed (waited 10000 usec)
[ 0.000000] omap_hwmod: i2c3: softreset failed (waited 10000 usec)
[ 0.000000] Reprogramming SDRC clock to 400000000 Hz
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts
[ 0.000000] Total of 96 interrupts on 1 active controller
[ 0.000000] GPMC revision 5.0
[ 0.000000] Trying to install interrupt handler for IRQ402
[ 0.000000] Trying to install interrupt handler for IRQ403
[ 0.000000] Trying to install interrupt handler for IRQ404
[ 0.000000] Trying to install interrupt handler for IRQ405
[ 0.000000] Trying to install interrupt handler for IRQ406
[ 0.000000] Trying to install interrupt handler for IRQ407
[ 0.000000] Trying to install interrupt handler for IRQ408
[ 0.000000] Trying to install type control for IRQ409
[ 0.000000] Trying to set irq flags for IRQ409
[ 0.000000] OMAP clockevent source: GPTIMER1 at 32768 Hz
[ 0.000000] Console: colour dummy device 80x30
[ 0.000000] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar
[ 0.000000] ... MAX_LOCKDEP_SUBCLASSES: 8
[ 0.000000] ... MAX_LOCK_DEPTH: 48
[ 0.000000] ... MAX_LOCKDEP_KEYS: 8191
[ 0.000000] ... CLASSHASH_SIZE: 4096
[ 0.000000] ... MAX_LOCKDEP_ENTRIES: 16384
[ 0.000000] ... MAX_LOCKDEP_CHAINS: 32768
[ 0.000000] ... CHAINHASH_SIZE: 16384
[ 0.000000] memory used by lock dependency info: 3935 kB
[ 0.000000] per task-struct memory footprint: 2304 bytes
[ 0.000000] Calibrating delay loop... 597.64 BogoMIPS (lpj=2334720)
[ 0.000000] pid_max: default: 32768 minimum: 301
[ 0.000000] Security Framework initialized
[ 0.000000] Mount-cache hash table entries: 512
[ 0.000000] CPU: Testing write buffer coherency: ok
[ 0.000000] regulator: core version 0.5
[ 0.000000] regulator: dummy:
[ 0.000000] NET: Registered protocol family 16
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.000000] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.000000] Switched to new clocking rate (Crystal/Core/MPU): 26.0/400/600 MHz
[ 0.000000] OMAP DMA hardware revision 5.0
[ 0.090759] bio: create slab <bio-0> at 0
[ 0.094268] regulator: vwl1271: 1800 mV
[ 0.098480] SCSI subsystem initialized
[ 0.107238] usbcore: registered new interface driver usbfs
[ 0.108306] usbcore: registered new interface driver hub
[ 0.109008] usbcore: registered new device driver usb
[ 0.112792] omap_i2c omap_i2c.1: bus 1 rev4.0 at 2600 kHz
[ 0.120208] twl4030: PIH (irq 7) chaining IRQs 368..375
[ 0.120330] twl4030: power (irq 373) chaining IRQs 376..383
[ 0.121978] twl4030: gpio (irq 368) chaining IRQs 384..401
[ 0.133972] regulator: VIO: 1800 mV normal standby
[ 0.135864] regulator: VMMC1: 1850 <--> 3150 mV at 3000 mV normal standby
[ 0.137756] regulator: VDAC: 1800 mV normal standby
[ 0.139648] regulator: VAUX2_4030: 2800 mV normal standby
[ 0.141510] regulator: VPLL2: 1800 mV normal standby
[ 0.143402] regulator: VSIM: 1800 <--> 3000 mV at 1800 mV normal standby
[ 0.145294] regulator: VAUX3: 2800 mV normal standby
[ 0.146179] omap_device: omap_i2c.1: new worst case deactivate latency 0: 30517
[ 0.146331] omap_device: omap_i2c.2: new worst case activate latency 0: 30517
[ 0.146453] omap_i2c omap_i2c.2: bus 2 rev4.0 at 400 kHz
[ 0.161834] omap_i2c omap_i2c.3: bus 3 rev4.0 at 400 kHz
[ 0.166564] Advanced Linux Sound Architecture Driver Version 1.0.23.
[ 0.168853] Bluetooth: Core ver 2.15
[ 0.169525] NET: Registered protocol family 31
[ 0.169525] Bluetooth: HCI device and connection manager initialized
[ 0.169647] Bluetooth: HCI socket layer initialized
[ 0.171081] Switching to clocksource 32k_counter
[ 0.266357] musb-hdrc: version 6.0, otg (peripheral+host), debug=0
[ 0.266693] musb-hdrc musb-hdrc.0: dma type: dma-inventra
[ 0.267395] musb-hdrc musb-hdrc.0: USB OTG mode controller at fa0ab000 using DMA, IRQ 92
[ 0.268707] NET: Registered protocol family 2
[ 0.269226] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.270294] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[ 0.270812] TCP bind hash table entries: 16384 (order: 7, 720896 bytes)
[ 0.275085] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.275146] TCP reno registered
[ 0.275177] UDP hash table entries: 256 (order: 2, 24576 bytes)
[ 0.275329] UDP-Lite hash table entries: 256 (order: 2, 24576 bytes)
[ 0.276000] NET: Registered protocol family 1
[ 0.277038] RPC: Registered udp transport module.
[ 0.277069] RPC: Registered tcp transport module.
[ 0.277069] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.277740] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.282897] omap3evm camera init done successfully...
[ 0.283477] omap-iommu omap-iommu.0: isp registered
[ 0.284118] AM37x/DM37x Linux PSP version 04.02.00.07 (OMAP3EVM)
[ 0.452423] VFS: Disk quotas dquot_6.5.2
[ 0.452606] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.454437] JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 0.455322] msgmni has been set to 966
[ 0.459472] io scheduler noop registered
[ 0.459503] io scheduler deadline registered
[ 0.459655] io scheduler cfq registered (default)
[ 0.523101] OMAP DSS rev 2.0
[ 0.523315] OMAP DISPC rev 3.0
[ 0.523406] OMAP VENC rev 2
[ 0.524230] OMAP DSI rev 1.0
[ 0.854675] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.860412] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 72) is a OMAP UART0
[ 1.611907] console [ttyO0] enabled
[ 1.616943] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 73) is a OMAP UART1
[ 1.625457] omap_uart.2: ttyO2 at MMIO 0x49020000 (irq = 74) is a OMAP UART2
[ 1.633880] omap_uart.3: ttyO3 at MMIO 0x49042000 (irq = 80) is a OMAP UART3
[ 1.675506] brd: module loaded
[ 1.695129] loop: module loaded
[ 1.705108] omap2-nand driver initializing
[ 1.709930] NAND device: Manufacturer ID: 0xad, Chip ID: 0xbc (Hynix )
[ 1.716888] Creating 5 MTD partitions on "omap2-nand.0":
[ 1.722534] 0x000000000000-0x000000080000 : "X-Loader-NAND"
[ 1.733978] 0x000000080000-0x0000001c0000 : "U-Boot-NAND"
[ 1.744720] 0x0000001c0000-0x000000280000 : "Boot Env-NAND"
[ 1.755371] 0x000000280000-0x000000780000 : "Kernel-NAND"
[ 1.767791] 0x000000780000-0x000020000000 : "File System - NAND"
[ 2.023864] OneNAND driver initializing
[ 2.028106] omap2-onenand omap2-onenand: Cannot request GPMC CS
[ 2.034545] omap2-onenand: probe of omap2-onenand failed with error -16
[ 2.044769] smsc911x: Driver version 2008-10-21.
[ 3.797210] irq 336: nobody cared (try booting with the "irqpoll" option)
[ 3.804351] [<c004fa88>] (unwind_backtrace+0x0/0xec) from [<c00b6a34>] (__report_bad_irq+0x30/0x8c)
[ 3.813873] [<c00b6a34>] (__report_bad_irq+0x30/0x8c) from [<c00b6bdc>] (note_interrupt+0x14c/0x1dc)
[ 3.823455] [<c00b6bdc>] (note_interrupt+0x14c/0x1dc) from [<c00b7938>] (handle_level_irq+0xe0/0x144)
[ 3.833160] [<c00b7938>] (handle_level_irq+0xe0/0x144) from [<c0066f74>] (gpio_irq_handler+0x13c/0x170)
[ 3.843017] [<c0066f74>] (gpio_irq_handler+0x13c/0x170) from [<c003f078>] (asm_do_IRQ+0x78/0xa0)
[ 3.852264] [<c003f078>] (asm_do_IRQ+0x78/0xa0) from [<c0481df4>] (__irq_svc+0x34/0x80)
[ 3.860687] Exception stack(0xdec2be08 to 0xdec2be50)
[ 3.865966] be00: c07bcda0 00000301 dec1a040 00000001 c07bcda0 60000013
[ 3.874572] be20: 00000000 00000150 c07bcda0 60000013 c07bcd84 00000088 0000006d dec2be50
[ 3.883148] be40: c0481bf8 c0481bfc 60000013 ffffffff
[ 3.888458] [<c0481df4>] (__irq_svc+0x34/0x80) from [<c0481bfc>] (_raw_spin_unlock_irqrestore+0x2c/0x34)
[ 3.898437] [<c0481bfc>] (_raw_spin_unlock_irqrestore+0x2c/0x34) from [<c00b61a4>] (__setup_irq+0x24c/0x320)
[ 3.908752] [<c00b61a4>] (__setup_irq+0x24c/0x320) from [<c00b6390>] (request_threaded_irq+0x118/0x168)
[ 3.918609] [<c00b6390>] (request_threaded_irq+0x118/0x168) from [<c0479598>] (smsc911x_drv_probe+0x6b4/0x1394)
[ 3.929229] [<c0479598>] (smsc911x_drv_probe+0x6b4/0x1394) from [<c027f240>] (platform_drv_probe+0x1c/0x24)
[ 3.939453] [<c027f240>] (platform_drv_probe+0x1c/0x24) from [<c027e10c>] (driver_probe_device+0xcc/0x1b4)
[ 3.949615] [<c027e10c>] (driver_probe_device+0xcc/0x1b4) from [<c027e25c>] (__driver_attach+0x68/0x8c)
[ 3.959472] [<c027e25c>] (__driver_attach+0x68/0x8c) from [<c027d864>] (bus_for_each_dev+0x4c/0x8c)
[ 3.968963] [<c027d864>] (bus_for_each_dev+0x4c/0x8c) from [<c027d118>] (bus_add_driver+0x104/0x290)
[ 3.978576] [<c027d118>] (bus_add_driver+0x104/0x290) from [<c027e584>] (driver_register+0xc0/0x150)
[ 3.988159] [<c027e584>] (driver_register+0xc0/0x150) from [<c003f3c8>] (do_one_initcall+0xc8/0x194)
[ 3.997772] [<c003f3c8>] (do_one_initcall+0xc8/0x194) from [<c000869c>] (kernel_init+0x98/0x150)
[ 4.006988] [<c000869c>] (kernel_init+0x98/0x150) from [<c004accc>] (kernel_thread_exit+0x0/0x8)
[ 4.016204] handlers:
[ 4.018585] [<c02c246c>] (smsc911x_irqhandler+0x0/0x558)
[ 4.024200] Disabling IRQ #336
[ 4.032470] smsc911x-mdio: probed
[ 4.036285] eth0: attached PHY driver [SMSC LAN8700] (mii_bus:phy_addr=ffffffff:01, irq=-1)
[ 4.045593] net eth0: MAC Address: 56:95:90:be:55:4e
[ 4.052124] usbcore: registered new interface driver asix
[ 4.058380] usbcore: registered new interface driver cdc_ether
[ 4.065093] usbcore: registered new interface driver net1080
[ 4.071624] usbcore: registered new interface driver cdc_subset
[ 4.078399] usbcore: registered new interface driver zaurus
[ 4.084289] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 5.093139] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
[ 5.099761] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
[ 5.108032] ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
[ 5.124420] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
[ 5.130950] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 5.138153] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 5.145782] usb usb1: Product: OMAP-EHCI Host Controller
[ 5.151458] usb usb1: Manufacturer: Linux 2.6.37-svn41 ehci_hcd
[ 5.157745] usb usb1: SerialNumber: ehci-omap.0
[ 5.165466] hub 1-0:1.0: USB hub found
[ 5.169464] hub 1-0:1.0: 3 ports detected
[ 5.203308] Initializing USB Mass Storage driver...
[ 5.209106] usbcore: registered new interface driver usb-storage
[ 5.215454] USB Mass Storage support registered.
[ 5.220977] usbcore: registered new interface driver usbtest
[ 5.227081] g_ether gadget: using random self ethernet address
[ 5.233245] g_ether gadget: using random host ethernet address
[ 5.240905] usb0: MAC 02:80:17:fb:3f:d5
[ 5.245086] usb0: HOST MAC de:9c:49:a8:6e:75
[ 5.249694] g_ether gadget: Ethernet Gadget, version: Memorial Day 2008
[ 5.256652] g_ether gadget: g_ether ready
[ 5.260925] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 5.266693] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[ 5.275207] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 5.282409] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 5.290039] usb usb2: Product: MUSB HDRC host driver
[ 5.295257] usb usb2: Manufacturer: Linux 2.6.37-svn41 musb-hcd
[ 5.301513] usb usb2: SerialNumber: musb-hdrc.0
[ 5.308746] hub 2-0:1.0: USB hub found
[ 5.312805] hub 2-0:1.0: 1 port detected
[ 5.320678] mice: PS/2 mouse device common for all mice
[ 5.329010] input: TWL4030 Keypad as /devices/platform/omap/omap_i2c.1/i2c-1/1-004a/twl4030_keypad/input/input0
[ 5.346832] ads7846 spi1.0: touchscreen, irq 335
[ 5.353607] input: ADS7846 Touchscreen as /devices/platform/omap2_mcspi.1/spi1.0/input/input1
[ 5.367858] input: twl4030_pwrbutton as /devices/platform/omap/omap_i2c.1/i2c-1/1-0049/twl4030_pwrbutton/input/input2
[ 5.382934] twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0
[ 5.389587] twl_rtc twl_rtc: Power up reset detected.
[ 5.395904] twl_rtc twl_rtc: Enabling TWL-RTC.
[ 5.402130] i2c /dev entries driver
[ 5.410217] Linux media interface: v0.10
[ 5.415100] Linux video capture interface: v2.00
[ 5.421966] omap3isp supply VDD_CSIPHY1 not found, using dummy regulator
[ 5.429229] omap3isp supply VDD_CSIPHY2 not found, using dummy regulator
[ 5.436614] omap3isp omap3isp: Revision 15.0 found
[ 5.441894] omap-iommu omap-iommu.0: isp: version 1.1
[ 5.515441] usb 1-2: new high speed USB device using ehci-omap and address 2
[ 5.523223] omap_device: omap_i2c.1: new worst case deactivate latency 0: 91552
[ 5.531188] mt9t111 2-003c: Unable to detectmt9t111sensor
[ 5.541168] isp_register_subdev_group: Unable to register subdev mt9t111
[ 5.549743] tvp514x 3-005c: tvp514x 3-005c decoder driver registered !!
[ 5.557922] tvp514x 3-005c: Write: retry ... 0
[ 5.585540] tvp514x 3-005c: Write: retry ... 1
[ 5.608947] tvp514x 3-005c: Write: retry ... 2
[ 5.632385] tvp514x 3-005c: Write: retry ... 3
[ 5.656005] tvp514x 3-005c: Write: retry ... 4
[ 5.679229] tvp514x 3-005c: Write: retry ... 5
[ 5.687622] usb 1-2: New USB device found, idVendor=0409, idProduct=005a
[ 5.694732] usb 1-2: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 5.703521] tvp514x 3-005c: Write failed. Err[-121]
[ 5.708648] tvp514x 3-005c: Unable to turn on decoder
[ 5.714752] tvp514x 3-005c: Read: retry ... 0
[ 5.720520] hub 1-2:1.0: USB hub found
[ 5.724639] hub 1-2:1.0: 4 ports detected
[ 5.741851] tvp514x 3-005c: Read: retry ... 1
[ 5.765197] tvp514x 3-005c: Read: retry ... 2
[ 5.788635] tvp514x 3-005c: Read: retry ... 3
[ 5.812103] tvp514x 3-005c: Read: retry ... 4
[ 5.835479] tvp514x 3-005c: Read: retry ... 5
[ 5.858947] tvp514x 3-005c: Unable to query std
[ 5.865020] usbcore: registered new interface driver uvcvideo
[ 5.871124] USB Video Class driver (v1.0.0)
[ 5.875885] omap_device: omap_wdt.-1: new worst case activate latency 0: 30517
[ 5.884735] OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
[ 5.891845] Bluetooth: HCI UART driver ver 2.2
[ 5.896514] Bluetooth: HCI H4 protocol initialized
[ 5.901702] Bluetooth: HCILL protocol initialized
[ 5.914825] mmci-omap-hs.1 supply vmmc_aux not found, using dummy regulator
[ 5.997741] usbcore: registered new interface driver usbhid
[ 6.003662] usbhid: USB HID core driver
[ 6.010040] usbcore: registered new interface driver snd-usb-audio
[ 6.020446] OMAP3 EVM SoC init
[ 6.109100] asoc: twl4030-hifi <-> omap-mcbsp-dai.1 mapping ok
[ 6.119201] ALSA device list:
[ 6.122314] #0: omap3evm
[ 6.125213] oprofile: hardware counters not available
[ 6.130523] oprofile: using timer interrupt.
[ 6.135223] nf_conntrack version 0.5.0 (7729 buckets, 30916 max)
[ 6.142944] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 6.148986] TCP cubic registered
[ 6.152374] Initializing XFRM netlink socket
[ 6.157043] NET: Registered protocol family 17
[ 6.161804] NET: Registered protocol family 15
[ 6.166900] Bluetooth: L2CAP ver 2.15
[ 6.170745] Bluetooth: L2CAP socket layer initialized
[ 6.176452] Bluetooth: SCO (Voice Link) ver 0.6
[ 6.181365] Bluetooth: SCO socket layer initialized
[ 6.187011] Bluetooth: RFCOMM TTY layer initialized
[ 6.192199] Bluetooth: RFCOMM socket layer initialized
[ 6.197631] Bluetooth: RFCOMM ver 1.11
[ 6.201568] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 6.207183] Bluetooth: BNEP filters: protocol multicast
[ 6.212707] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 6.220489] Registering the dns_resolver key type
[ 6.225860] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 6.235015] ThumbEE CPU extension supported.
[ 6.251983] Power Management for TI OMAP3.
[ 6.256866] sr_init: No PMIC hook to init smartreflex
[ 6.262664] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver initialized
[ 6.271545] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver initialized
[ 6.280883] SmartReflex Class3 initialized
[ 6.319000] clock: disabling unused clocks to save power
[ 6.326202] platform mpu.0: omap_voltage_scale: Already at the requestedrate 600000000
[ 6.338439] fbcvt: 1024x768@60: CVT Name - .786M3-R
[ 6.358520] regulator_init_complete: incomplete constraints, leaving VDAC on
[ 6.367828] twl_rtc twl_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
[ 6.376770] omap_vout omap_vout: Buffer Size = 3686400
[ 6.384307] omap_vout omap_vout: : registered and initialized video device 16
[ 6.391906] omap_vout omap_vout: Buffer Size = 3686400
[ 6.399200] omap_vout omap_vout: : registered and initialized video device 17
[ 6.410644] yaffs: dev is 32505860 name is "mtdblock4" rw
[ 6.416412] yaffs: passed flags ""
[ 13.366119] VFS: Mounted root (yaffs2 filesystem) on device 31:4.
[ 13.372741] Freeing init memory: 220K
[ 13.419891] Kernel panic - not syncing: Attempted to kill init!
[ 13.426208] [<c004fa88>] (unwind_backtrace+0x0/0xec) from [<c047e708>] (panic+0x4c/0x180)
[ 13.434875] [<c047e708>] (panic+0x4c/0x180) from [<c007c60c>] (do_exit+0x6c/0x644)
[ 13.442871] [<c007c60c>] (do_exit+0x6c/0x644) from [<c007cc74>] (do_group_exit+0x90/0xc0)
[ 13.451507] [<c007cc74>] (do_group_exit+0x90/0xc0) from [<c008ad9c>] (get_signal_to_deliver+0x39c/0x3ec)
[ 13.461517] [<c008ad9c>] (get_signal_to_deliver+0x39c/0x3ec) from [<c004c964>] (do_notify_resume+0x70/0x62c)
[ 13.471862] [<c004c964>] (do_notify_resume+0x70/0x62c) from [<c0049cf8>] (work_pending+0x24/0x28)