This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Beaglebone Black 的LCD 分辨率 1280 X 800 kernel 不能正常启动 (Android 4.2.2 安卓系统)

大家好,

我根据文档 http://processors.wiki.ti.com/index.php/TI-Android-JB-4.2.2-DevKit-4.1.1_DeveloperGuide 下载的Android源码并进行了编译.

在Beaglebone Black 下运行, 配置 内核3.2 (driver/video/da8xx-fb.c) TFT-LCD 480 X 272 和 800 X 480 分辨率都能正常工作, 但是 配置1280 X 800分辨率的时候,BBB不能正常启动,报错如下,请问我应该如何解决? 

> root@android:/ # [   5.018737] Disabling lock debugging due to kernel taint

> [   5.066040] omaplfb: OMAPLFB_Init: OMAPLFBInit failed

> [   6.284454] init: untracked pid 70 exited

> [   9.568054] init: untracked pid 236 exited

多谢!

Kind Regards,

Jerry