DM365,W25Q128的flash,rootfs是squashfs格式时跑到Please press Enter to activate this console.都要20秒,rootfs是jffs2格式时跑到Please press Enter to activate this console.时甚至要1分钟左右,而且没有报任何错误,有人遇到过类似的情况吗,感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DM365,W25Q128的flash,rootfs是squashfs格式时跑到Please press Enter to activate this console.都要20秒,rootfs是jffs2格式时跑到Please press Enter to activate this console.时甚至要1分钟左右,而且没有报任何错误,有人遇到过类似的情况吗,感谢。
但是这个jffs2文件系统才6M大小,而同样加载到Freeing init memory: 100K时,在SPI FLASH要30秒,在NAND FLASH只要9秒而已。这合理吗。谢谢你。
还发现,进入jffs2文件系统后,创建目录失败,提示说文件系统只读。
| SPI FLASH | SPI FLASH | NAND FLASH | NAND FLASH | |
| rootfs格式 | jffs2 | squashfs | jffs2 | squashfs |
| Freeing init memory | 30s | 3s | 9s | 3s |
你好,
在你的ubl里面,是否有把SPI相关时钟配置为芯片支持的最高频率?是否有使能DMA进行数据搬移?