Other Parts Discussed in Thread: SYSBIOS
我使用的是例程uart2,首先这个例程是没有问题的,CCS工程也是没有问题的,因为我在开发板上可以正常进入debug模式,也可以正常启动;
有硬件工程师提供的两套板子,板子的设计是一样的,参考创龙核心板的设计;
现在遇到的问题是:
在一块板子上,可以正常的进入debug模式;另一块板子提示如下错误:
C674X_0: File Loader: Verification failed: Values at address 0xC0103060 do not match Please verify target memory and memory map.
C674X_0: GEL: File: D:\share\DSP\demo\SYSBIOS\Application\UART2\Debug\UART2.out: a data verification error occurred, file load failed.

我又测试 test 测试XDS V2 连接,是成功的;
[Start: Texas Instruments XDS100v2 USB Emulator_0]
-----[Perform the Integrity scan-test on the JTAG DR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG DR Integrity scan-test has succeeded.
[End: Texas Instruments XDS100v2 USB Emulator_0]