This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am4379启动后app不能启动



我是参考AM4379-evm设计的板卡;目前启动系统时能正常显示启动界面,进入系统后无法启动app,打印信息如下:

Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Starting rpcbind daemon...done.
creating NFS state directory: done
starting statd: done
hwclock: can't open '/dev/misc/rtc': No such file or directory
Starting syslogd/klogd: done
Starting thttpd.
ioctl FBIOPUT_VSCREENINFO: Invalid argument
Starting PVR
find: /lib/modules/4.9.69-g9ce43c71ae: No such file or directory
insmod: ERROR: missing filename.
Could not find pvrsrvkm driver
Starting Lighttpd Web Server: lighttpd.
2015-07-06 21:15:09: (/home/gtbldadm/ti/oe-layersetup/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/cortexa9t2hf-vfp-neon-linux-gnueabi/lighttpd/1.4.33-r1/lighttpd-1.4.33/src/log.c.166) server started
/
Starting Matrix GUI application.
Enabling thermal zones...
/etc/rc5.d/S98thermal-zone-init: line 7: /sys/class/thermal/thermal_zone*/mode: No such file or directory
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
autoconf
binutils
cpp-symlinks
cpp
g++-symlinks
g++
gcc-symlinks
gcc
gdbserver
gstreamer1.0-libav
libgmp10
libmpc3
libmpfr4
make

If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
Stopping Bootlog daemon: bootlogd.

_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|

Arago Project http://arago-project.org am437x-evm /dev/ttyO0

Arago 2015.05 am437x-evm /dev/ttyO0