This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6638 ARM和DSP核之间的通信

IT工程师你们好:

       我们现在使用官网提供的C6638开发板,DSP有8个核,ARM有4个核。存在问题

     1). ARM第一个核跑LINUX操作系统,请问如何在linux中使用剩余的三个ARM核,将其启动使用。

     2).在DSP开发中,8个DSP核之间的通信采用队列,请问ARM跑LINUX起来后如何实现和DSP8个核之间的数据交换,可以通过几种方式时间核间数据交互,那种方式的速度最快。