Hi,TI guys:
我在使用C6678 EVM运行论坛上KeyStone_SRIO的测试程序,在interrupt配置中程序将srio的中断配给了INT4,然后将doorbell中断配置到了core0. 但是我并没有看到中断响应函数doorbell_isr和这个doorbell中断相关联的语句,类似于中断有一个就中断响应函数名字的语句。我想问一下,这个配置到了core0的doorbell中断在core0中时如何响应的?doorbell中断响应函数是如何配置达到与对应doorbell相关联的?另外,在keystone相关文档中,我看到doorbell章节中说系统通过tid决定收到doorbell后的操作,但我在KeyStone_SRIO的代码中并没有找到与doorbell相关的代码。如何去响应一个doorbell??