This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM57x 功耗与散热问题

Other Parts Discussed in Thread: AM5728

HI TI工程师们:

在使用 AM5728 + A7 设计一款手持式产品时遇到了瓶颈:由于机构为封闭式塑料外壳,板上器件(CPU)工作时发出的热量不能散发出去,温度与功耗双增加,最终导致CPU过热关闭。

AM5728我们采用核心板形式,功耗主要集中在 CPU、PMIC、DDR

我们使用了TI 关于AM5728的功耗评估表进行功耗优化。根据评估表,最终优化结果 CPU 功耗为 2.8W,相应PMIC功耗为0.67W,4片DDR为0.5W。 核心板功耗4W。

在未装机壳,裸板运行时,核心板功耗实测也是在4W左右(带散热片),FPGA + 其他外设约占6.5W。整板10.5W功耗。

但整板10.5W是在裸板运行时的功耗。一旦装上机壳,运行一段时间之后,随着CPU温度上升,功耗也会逐渐增加,最终功耗将超过12W,CPU过热关闭。

问题:

1、CPU以及其他芯片,是否温度越高,功耗也会相应的增加? 

2、若是,如此形成的正反馈将不断推高功耗与温度,最终导致CPU过热关闭,要如何避免或打破这个正反馈(已加散热片)?

3、密闭塑料外壳的手持式设备,要如何考虑散热?