This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS load memory失败



在CCS软件中使用load memory将数据写到DDR3中,但是load进去的数据总是不对,注意,在之前我已经配置过DDR3了,没有错误,可以在memory browser中手动的改动DDR3地址中的数据,但是使用load memory就不对。见下图。

上图中的DDR3空间中的数据全部是0x5a5a5a5a,测试DDR3使用的数据

上图中,加载的数据是IBL配置的bin文件

设置起始地址,位宽

load memory后,在memory窗口中不会自动刷新,手动刷新后,数据和上图中的bin文件内容不同

重新将数据load共享ram中,正确。0x0c000000开头的空间。

是我DDR3配置不正确吗?这个是我自己的板子,但是我已经使用数据对很大的一段空间(绝对大于看load的bin文件大小)中的数据进行过测试,读写都正确,但是load就是不正确,load后不自动刷新,手动刷新后,数据和需要load的文件(配置IBL的i2crom_0x51_c6678_le.bin)内容不同,有人碰到过吗,感谢!