This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm8148PVR打开失败,急求高手指教



用的是8148的板子,最近启动时出现问题了,打不开PVR。急求高手指教!

INIT: version 2.86 booting
Please wait: booting...
Error opening /dev/fb0: No such file or directory
Starting udev
udevd (77): /proc/77/oom_adj is deprecated, please use /proc/77/oom_score_adj in
stead.
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p3): warning: maximal mount count reached, running e2fsck is rec
ommended
EXT3-fs (mmcblk0p3): using internal journal
EXT3-fs (mmcblk0p3): recovery complete
EXT3-fs (mmcblk0p3): mounted filesystem with writeback data mode
Remounting root file system...
Caching udev devnodes
NET: Registered protocol family 10
ALSA: Restoring mixer settings...
Configuring network interfaces... ifconfig: SIOCGIFFLAGS: No such device
done.
Setting up IP spoofing protection: rp_filter.
Fri Nov 11 09:35:00 UTC 2011
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
open /dev/fb0: No such file or directory
open /dev/fb0: No such file or directory
expr: syntax error
Linux Frame Buffer Device Configuration Version 2.1 (23/06/1999)
(C) Copyright 1995-1999 by Geert Uytterhoeven


Usage: fbset [options] [mode]

Valid options:
General options:
-h, --help : display this usage information
--test : don't change, just test whether the mode is valid
-s, --show : display video mode settings
-i, --info : display all frame buffer information
-v, --verbose : verbose mode
-V, --version : print version information
-x, --xfree86 : XFree86 compatibility mode
-a, --all : change all virtual consoles on this device
Frame buffer special device nodes:
-fb <device> : processed frame buffer device
(default is /dev/fb0)
Video mode database:
-db <file> : video mode database file
(default is /etc/fb.modes)
Display geometry:
-xres <value> : horizontal resolution (in pixels)
-yres <value> : vertical resolution (in pixels)
-vxres <value> : virtual horizontal resolution (in pixels)
-vyres <value> : virtual vertical resolution (in pixels)
-depth <value> : display depth (in bits per pixel)
-nonstd <value> : select nonstandard video mode
-g, --geometry ... : set all geometry parameters at once
-match : set virtual vertical resolution by virtual resolution
Display timings:
-pixclock <value> : pixel clock (in picoseconds)
-left <value> : left margin (in pixels)
-right <value> : right margin (in pixels)
: lower margin (in pixel lines)
-hslen <value> : horizontal sync length (in pixels)
-vslen <value> : vertical sync length (in pixel lines)
-t, --timings ... : set all timing parameters at once
Display flags:
-accel <value> : hardware text acceleration enable (false or true)
-hsync <value> : horizontal sync polarity (low or high)
-vsync <value> : vertical sync polarity (low or high)
-csync <value> : composite sync polarity (low or high)
-gsync <value> : synch on green (false or true)
-extsync <value> : external sync enable (false or true)
-bcast <value> : broadcast enable (false or true)
-laced <value> : interlace enable (false or true)
-double <value> : doublescan enable (false or true)
-rgba <r,g,b,a> : recommended length of color entries
-grayscale <value> : grayscale enable (false or true)
Display positioning:
-move <direction> : move the visible part (left, right, up or down)
-step <value> : step increment (in pixels or pixel lines)
(default is 8 horizontal, 2 vertical)
Starting PVR
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
VPSS_CORE : Failed to init fvid2 interface,
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver
FATAL: Error inserting omaplfb (/lib/modules/2.6.37/kernel/drivers/gpu/pvr/omapl
fb.ko): No such device
/dev/mem opened.
Memory mapped at address 0x401a1000.
Read at address 0x48180F04 (0x401a1f04): 0x00000001
Write at address 0x48180F04 (0x401a1f04): 0x00000000, readback 0x00000000
/dev/mem opened.
Memory mapped at address 0x4031c000.
Read at address 0x48180900 (0x4031c900): 0x00000102
Write at address 0x48180900 (0x4031c900): 0x00000002, readback 0x00000002
/dev/mem opened.
Memory mapped at address 0x400d1000.
Read at address 0x48180920 (0x400d1920): 0x00040002
Write at address 0x48180920 (0x400d1920): 0x00000002, readback 0x00000002
Starting Matrix GUI application.