This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS4.1.2连接C6472问题



使用合众达SEED-XDS560plus仿真器将C6472连至CCSv4.1.2时弹出如下所示error

Error connecting to the target:
Error 0x00000020/-2172
Error during: Execution,
TRG_ERR_COMM_FAILURE Error Occured at 0x0000000D

晶振都正常

请问此问题如何解决

 

  • 1  首先确保仿真器驱动已经正常安装,可以在我的电脑里查看

    2  你的配置文件是什么?

    3  更换其他EVM板,是否能正常链接上

    4  6472是自己做的板子吗?若是,请首先检查上电和时钟,再调试JTAG

  • Hi,板子已能连上,现在run简单的hello world程序时弹出error

    C64XP: Trouble Writing Memory Block at 0x20 on Page 0 of Length 0x66c0: Error 0x00000002/-1190 Error during: Memory,  The DTDMA memory request is not serviced by the HW memory system.  This could be caused by the memory address specified does not exist in the specified  memory/cache level.  
    Cannot write to target

    请问此问题怎么处理

     

  • 你好,我也出现了你这种情况,不过我用的是CCS3.3.83.20的软件,但是一直连接不上,XDS560Plus上的灯刚开始也是亮的,连接的时候就是一直报Error connecting to the target: Error 0x00000020/-2172 Error during: Execution,  TRG_ERR_COMM_FAILURE Error Occur,请问你的解决了么?是怎么解决的?谢谢