TMS320C6748核心板,采用3路独立电源供电,上电次序依次为+5V、+1.3V、+1.8V和3.3V,各个电源上电的时间间隔在200us左右,采用24MHz无源晶振,实测晶振正常起振,输出24MHz时钟信号,复位芯片采用tps3808g33dbvr,在3.3V正常供电后保持200ms低电平以供CPU复位,采用CC6.0平台进行编译时,报错
PSC0 Enable Transition Timeout on Domain 0 ,LPSC0
PSC0 Enable Verify Timeout on Domain 0,LPSC0
PSC0 Enable Transition Timeout on Domain 0,LPSC1
PSC0 Enable Verify Timeout on Domain 0,LPSC1
PSC0 Enable Transition Timeout on Domain 0,LPSC2
PSC0 Enable Verify Timeout on Domain 0,LPSC2
PSC0 Enable Transition Timeout on Domain 0,LPSC3
PSC0 Enable Verify Timeout on Domain 0,LPSC3
PSC0 Enable Transition Timeout on Domain 0,LPSC4
PSC0 Enable Verify Timeout on Domain 0,LPSC4
PSC0 Enable Transition Timeout on Domain 0,LPSC5
PSC0 Enable Verify Timeout on Domain 0,LPSC5
PSC0 Enable Transition Timeout on Domain 0,LPSC9
PSC0 Enable Verify Timeout on Domain 0,LPSC9
PSC1 Enable Transition Timeout on Domain 0,LPSC0
PSC1 Enable Verify Timeout on Domain 0,LPSC0
PSC1 Enable Transition Timeout on Domain 0,LPSC1
PSC1 Enable Verify Timeout on Domain 0,LPSC1
PSC1 Enable Transition Timeout on Domain 0,LPSC2
PSC1 Enable Verify Timeout on Domain 0,LPSC2
......
PSC1 Enable Transition Timeout on Domain 0,LPSC21
PSC1 Enable Verify Timeout on Domain 0,LPSC21
PSC1 Enable Transition Timeout on Domain 0,LPSC31
PSC1 Enable Verify Timeout on Domain 0,LPSC31
PSC Enable
---------------------------------------------------------------------------
PLL0 init done for Core:456MHz,EMIFA:45MHz
DDR initialization is in progress...
--------------------------------------------------------------------------
C674x_0:Trouble Reading Memory Block at 0x1c188 on Page 0 of Length 0x4:(Error-1178@0x1C14188 ) Device functional clock
configuration and/or try more reliable JTAG(e.g.lower TCLK)(Emulation package 5.1.507.0)
C674X_0:GEL:Eror while executing OntargetConnect():Target failed to read 0x01C14188 at(*(unsigned int*)(0x01C141000))
2) [TH8300.gel:439] at Set_ DDRPLL_156MHz()
[TH8300.gel.447] at Set_DDR2_156MHz()
[TH8300.gel.454] at Core_456MHz_DDR2
at OnTargetconnect().
C674X_0:Trouble Reading Register CSR:(Error-1178@0x41)Device functional clock appears to be off.
Power-cycle the board.......
C674X_0:Trouble Writing Memory Block at 0xc0000000 on Page 0 of Length 0x80:(Error-1178@0x41188)Device functional clock
configuration and/or try more reliable JTAG(e.g.lower TCLK)(Emulation package 5.1.507.0)
C674X_0:GEl:File:D:\TH8300_prj_dsp\TH8300_prj\TH8300\Debug\TH8300.out:Load Failed