This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6657 SPI BOOT失败



使用SPI NOR FLASH直接加载,燒写成功,在线时,从flash中可以读出数据并校验成功。但在spi boot模式下,发现SPI FLASH并没有数据输出,修改SPI的时序,即调整bootmode[12:11]的设置,DSP只能从flash中读出parameter table字节,之后不再读flash数据,DSP就处于hung,并且SYSCLKOUT频率与设置的频率不同。不知道是什么问题,希望大神们回复一下,谢谢!

同样燒写加载在C6657的开发板上是成功的。