This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教:IAR编译出的文件没法SD卡启动??



实验条件如下:

1、AM335X_StarterWare_02_00_01_01打了BeagleBone Black的补丁。

2、IAR工程编译过程出现报警(Error[Lp049]: there was no reference to __iar_data_init3, but it is needed to initialize section .bss ....),修改了.icf文件 ,把 do not initialize  { section .noinit }; 改成了 do not initialize  { section .bss };(参考文章e2echina.ti.com/.../97888 ),消除编译报警。

问题如下:

 1、在BeagleBone Black上跑StarterWare的GPIO测试程序,在CSS和IAR上通过JTAG调试都没问题。
 2、SD卡启动,CSS编译出来的MLO和app拷入SD卡,SD卡启动,程序正常跑;IAR编译出来的MLO(boot_ti.bin)和app(gpioLEDBlink_ti.bin)拷入SD卡,无法启动,IAR编译出来的MLO和app文件都查过,加了TI的头信息。
哪位遇到这样的情况,麻烦给解答一下?不知是否与上述修改.icf文件消除编译报警有关?
谢谢!!!!