This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omap138 sdio通信失败



你好,TI专家,我们sdio连接wifi w18xx,但是在加载wifi时候发现,sdio写接口一直返回错误,错误码是-84,我们配置sdio的clk是1M,但是量到才300K不到,请问下,可能是什么原因,我们mmc0 是ok的,mmc1是接wifi的有问题,mmc0配置如下:

static struct davinci_mmc_config da850_wl12xx_mmc_config = {
.set_power = wl12xx_set_power,
.wires = 4,
.max_freq = 1000000,
.caps = MMC_CAP_4_BIT_DATA | MMC_CAP_POWER_OFF_CARD,
.version = MMC_CTLR_VERSION_2,
};

static const short da850_wl12xx_pins[] __initconst = {
DA850_MMCSD1_DAT_0, DA850_MMCSD1_DAT_1, DA850_MMCSD1_DAT_2,
DA850_MMCSD1_DAT_3, DA850_MMCSD1_CLK, DA850_MMCSD1_CMD,
DA850_GPIO6_7, DA850_GPIO6_6,
-1
};