有个很奇怪的现象:
ti sdk 提供了两种文件系统,一种精简版,一种完整版。
当使用完整版文件系统,启动后输入date 或hwclock 这类时间命令后,硬断电重启,无法加载内核模块。(reset软复位没问题)
使用精简版本也没有这个问题。
请问可能是什么原因呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有个很奇怪的现象:
ti sdk 提供了两种文件系统,一种精简版,一种完整版。
当使用完整版文件系统,启动后输入date 或hwclock 这类时间命令后,硬断电重启,无法加载内核模块。(reset软复位没问题)
使用精简版本也没有这个问题。
请问可能是什么原因呢?
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.19 (root@Woods) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #56 SMP PREEMPT Mon Jul 2 11:27:06 CST 2018
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI AM572x EVM Rev A3
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009f000000, size 8 MiB
[ 0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 80 MiB at 0x00000000fac00000
[ 0.000000] Forcing write-allocate cache policy for SMP
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] OMAP4: Map 0x00000000ffd00000 to fe600000 for dram barrier
[ 0.000000] DRA752 ES2.0
[ 0.000000] PERCPU: Embedded 11 pages/cpu @eed32000 s14848 r8192 d22016 u45056
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 472640
[ 0.000000] Kernel command line: console=ttyS0,115200n8 root=PARTUUID=0005d21a-02 rw rootfstype=ext4 rootwait video=HDMI-A-1:1024x768M@60
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 1623328K/1897472K available (6571K kernel code, 359K rwdata, 2392K rodata, 336K init, 290K bss, 28384K reserved, 245760K cma-reserved, 1225728K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08c904c (8965 kB)
[ 0.000000] .init : 0xc08ca000 - 0xc091e000 ( 336 kB)
[ 0.000000] .data : 0xc091e000 - 0xc0977c70 ( 360 kB)
[ 0.000000] .bss : 0xc0979000 - 0xc09c1ac0 ( 291 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] Architected cp15 timer(s) running at 6.14MHz (virt).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000004] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000015] Switching to timer-based delay loop, resolution 162ns
[ 0.000346] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000354] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000763] Console: colour dummy device 80x30
[ 0.000784] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000798] pid_max: default: 32768 minimum: 301
[ 0.000893] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000903] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001443] Initializing cgroup subsys io
[ 0.001460] Initializing cgroup subsys memory
[ 0.001483] Initializing cgroup subsys devices
[ 0.001496] Initializing cgroup subsys freezer
[ 0.001507] Initializing cgroup subsys perf_event
[ 0.001519] Initializing cgroup subsys pids
[ 0.001544] CPU: Testing write buffer coherency: ok
[ 0.001742] /cpus/cpu@0 missing clock-frequency property
[ 0.001759] /cpus/cpu@1 missing clock-frequency property
[ 0.001770] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.001805] Setting up static identity map for 0x800082c0 - 0x80008318
[ 0.080081] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.080141] Brought up 2 CPUs
[ 0.080154] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[ 0.080160] CPU: All CPU(s) started in SVC mode.
[ 0.080529] devtmpfs: initialized
[ 0.108057] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.109004] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.312387] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.317363] pinctrl core: initialized pinctrl subsystem
[ 0.318219] NET: Registered protocol family 16
[ 0.319133] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.350225] cpuidle: using governor ladder
[ 0.380254] cpuidle: using governor menu
[ 0.388899] OMAP GPIO hardware version 0.1
[ 0.420859] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.420870] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.421322] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.421332] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.421895] OMAP DMA hardware revision 0.0
[ 0.454521] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver
[ 0.455631] edma 43300000.edma: memcpy is disabled
[ 0.460455] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.464132] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.464316] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.464472] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.464624] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.464895] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 0.465076] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 0.467935] palmas 0-0058: Irq flag is 0x00000008
[ 0.482582] palmas 0-0058: Muxing GPIO 2f, PWM 0, LED 0
[ 0.563320] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.563818] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.564022] media: Linux media interface: v0.10
[ 0.564077] Linux video capture interface: v2.00
[ 0.564122] pps_core: LinuxPPS API ver. 1 registered
[ 0.564129] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.564155] PTP clock support registered
[ 0.564207] EDAC MC: Ver: 3.0.0
[ 0.564965] omap-mailbox 4883c000.mailbox: omap mailbox rev 0x400
[ 0.565257] omap-mailbox 4883e000.mailbox: omap mailbox rev 0x400
[ 0.565549] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.565835] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.566165] Advanced Linux Sound Architecture Driver Initialized.
[ 0.567007] clocksource: Switched to clocksource arch_sys_counter
[ 0.577848] NET: Registered protocol family 2
[ 0.578341] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.578405] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.578530] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.578576] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.578607] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.578748] NET: Registered protocol family 1
[ 0.579015] RPC: Registered named UNIX socket transport module.
[ 0.579025] RPC: Registered udp transport module.
[ 0.579031] RPC: Registered tcp transport module.
[ 0.579037] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.580066] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.582439] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.590202] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.590854] NFS: Registering the id_resolver key type
[ 0.590880] Key type id_resolver registered
[ 0.590887] Key type id_legacy registered
[ 0.591083] fuse init (API version 7.23)
[ 0.593148] bounce: pool size: 64 pages
[ 0.593199] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
[ 0.593215] io scheduler noop registered
[ 0.593228] io scheduler deadline registered
[ 0.593262] io scheduler cfq registered (default)
[ 0.598258] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[ 0.602301] PCI host bridge /ocp/axi@0/pcie@51000000 ranges:
[ 0.602312] No bus range found for /ocp/axi@0/pcie@51000000, using [bus 00-ff]
[ 0.602345] IO 0x20003000..0x20012fff -> 0x00000000
[ 0.602365] MEM 0x20013000..0x2fffffff -> 0x20013000
[ 0.632756] dra7-pcie 51000000.pcie: link is not up
[ 0.632929] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[ 0.632942] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.632953] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 0.632962] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 0.633371] PCI: bus0: Fast back to back transfers disabled
[ 0.633490] PCI: bus1: Fast back to back transfers enabled
[ 0.633539] irq: no irq domain found for /ocp/axi@0/pcie@51000000/interrupt-controller !
[ 0.633572] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 0.633586] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 0.633599] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.633824] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 0.695476] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.698882] console [ttyS0] disabled
[ 0.698934] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 301, base_baud = 3000000) is a 8250
[ 1.619094] console [ttyS0] enabled
[ 1.623485] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 302, base_baud = 3000000) is a 8250
[ 1.633162] 48422000.serial: ttyS7 at MMIO 0x48422000 (irq = 303, base_baud = 3000000) is a 8250
[ 1.642847] 4ae2b000.serial: ttyS9 at MMIO 0x4ae2b000 (irq = 304, base_baud = 3000000) is a 8250
[ 1.652923] [drm] Initialized drm 1.1.0 20060810
[ 1.659945] OMAP DSS rev 6.1
[ 1.663979] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 1.672529] omapdss_dss 58000000.dss: bound 58040000.encoder (ops hdmi5_component_ops)
[ 1.688545] loop: module loaded
[ 1.691959] at24 0-0050: 4096 byte 24c32 EEPROM, writable, 1 bytes/write
[ 1.701701] libphy: Fixed MDIO Bus: probed
[ 1.757040] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 1.763163] libphy: 48485000.mdio: probed
[ 1.771267] davinci_mdio 48485000.mdio: phy[1]: device 48485000.mdio:01, driver Micrel KSZ9031 Gigabit PHY
[ 1.781009] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver Micrel KSZ9031 Gigabit PHY
[ 1.791222] cpsw 48484000.ethernet: Detected MACID = 94:e3:6d:42:8f:f6
[ 1.798547] cpsw 48484000.ethernet: cpsw: Detected MACID = 94:e3:6d:42:8f:f7
[ 1.807103] mousedev: PS/2 mouse device common for all mice
[ 1.813147] i2c /dev entries driver
[ 1.819063] tmp102 0-0048: initialized
[ 1.825591] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 1.830503] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr104 mode
[ 1.836974] omap_hsmmc 4809c000.mmc: no pinctrl state for ddr50 mode
[ 1.843372] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr50 mode
[ 1.849768] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr25 mode
[ 1.856148] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr12 mode
[ 1.862546] omap_hsmmc 4809c000.mmc: no pinctrl state for hs mode
[ 1.868930] vdd_3v3: supplied by regen1
[ 1.917518] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 1.923900] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 1.988489] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.999465] NET: Registered protocol family 10
[ 2.014763] sit: IPv6 over IPv4 tunneling driver
[ 2.020017] NET: Registered protocol family 17
[ 2.024696] Key type dns_resolver registered
[ 2.029114] omap_voltage_late_init: Voltage driver support not added
[ 2.035991] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.042244] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.048942] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.055150] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.063283] Power Management for TI OMAP4+ devices.
[ 2.068392] Registering SWP/SWPB emulation handler
[ 2.075227] dmm 4e000000.dmm: initialized all PAT entries
[ 2.085153] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.091809] [drm] No driver support for vblank timestamp query.
[ 2.097772] omapdrm omapdrm.0: No connectors reported connected with modes
[ 2.104677] [drm] Cannot find any crtc or sizes - going 1024x768
[ 2.113292] [drm] Enabling DMM ywrap scrolling
[ 2.122160] Console: switching to colour frame buffer device 128x48
[ 2.132212] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
[ 2.152556] mmc0: host does not support reading read-only switch, assuming write-enable
[ 2.160665] mmc0: new SDHC card at address 0001
[ 2.165528] mmcblk0: mmc0:0001 ASTC 7.44 GiB
[ 2.170580] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
[ 2.172122] mmcblk0: p1 p2
[ 2.187954] aaaaaaaaa
[ 2.199941] hctosys: unable to open rtc device (rtc0)
[ 2.213047] aic_dvdd_fixed: disabling
[ 2.216897] ldousb: disabling
[ 2.220289] ALSA device list:
[ 2.223267] No soundcards found.
[ 2.260476] mmc1: MAN_BKOPS_EN bit is not set
[ 2.452100] bbbbbbbbbb
[ 2.454733] cccccccccccc
[ 2.457659] mmc1: new DDR MMC card at address 0001
[ 2.473068] mmcblk1: mmc1:0001 R1J56L 13.8 GiB
[ 2.487970] mmcblk1boot0: mmc1:0001 R1J56L partition 1 16.0 MiB
[ 2.504227] mmcblk1boot1: mmc1:0001 R1J56L partition 2 16.0 MiB
[ 2.510980] mmcblk1: p1 p2
[ 3.545402] EXT4-fs (mmcblk0p2): 4 orphan inodes deleted
[ 3.550775] EXT4-fs (mmcblk0p2): recovery complete
[ 3.609771] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 3.617942] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 3.626017] devtmpfs: mounted
[ 3.629210] Freeing unused kernel memory: 336K (c08ca000 - c091e000)
[ 3.635592] This architecture does not have kernel memory protection.
[ 4.031768] systemd[1]: System time before build time, advancing clock.
[ 4.090008] random: systemd: uninitialized urandom read (16 bytes read, 24 bits of entropy available)
[ 4.105319] random: systemd: uninitialized urandom read (16 bytes read, 24 bits of entropy available)
[ 4.116989] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 4.135505] systemd[1]: Detected architecture arm.
Welcome to Arago 2016.08!
[ 4.169411] systemd[1]: Set hostname to <tky_v2>.
[ 4.300032] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 4.304159] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 4.304338] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 4.347757] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 26 bits of entropy available)
[ 4.401499] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 27 bits of entropy available)
[ 4.567039] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 4.576517] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 4.586385] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 5.321021] systemd[1]: sysinit.target: Found ordering cycle on sysinit.target/start
[ 5.328848] systemd[1]: sysinit.target: Found dependency on alignment.service/start
[ 5.336543] systemd[1]: sysinit.target: Found dependency on basic.target/start
[ 5.343862] systemd[1]: sysinit.target: Found dependency on sysinit.target/start
[ 5.351325] systemd[1]: sysinit.target: Breaking ordering cycle by deleting job alignment.service/start
[ 5.360780] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with sysinit.target/start
[ SKIP ] Ordering cycle found, skipping alignment.service
[ 5.399510] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 5.427239] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 5.457239] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 5.477254] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 5.507239] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 5.538410] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 5.567293] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 5.637231] systemd[1]: Mounting Temporary Directory...
Mounting Temporary Directory...
[ 5.669319] systemd[1]: Mounting Debug File System...
Mounting Debug File System...
[ 5.727235] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 5.757288] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 5.777351] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 5.837621] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 5.867948] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 5.927450] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 5.951292] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 5.957270] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 5.989919] systemd[1]: Starting Create Static Device Nodes in /dev...
Starting Create Static Device Nodes in /dev...
[ 6.017993] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 6.047280] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 6.067202] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 6.087444] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 6.187604] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 6.220640] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 6.248028] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 6.277207] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 6.335043] systemd[1]: Mounted Debug File System.
[ OK ] Mounted Debug File System.
[ 6.367242] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 6.397184] systemd[1]: Mounted Temporary Directory.
[ OK ] Mounted Temporary Directory.
[ 6.417356] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Started Setup Virtual Console.
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Started Create Static Device Nodes in /dev.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
Starting Apply Kernel Variables...
Mounting FUSE Control File System...
Starting udev Kernel Device Manager...
Starting udev Coldplug all Devices...
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
Mounting /media/ram...
Starting Flush Journal to Persistent Storage...
[ OK ] Mounted FUSE Control File System.
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Apply Kernel Variables.
[ 7.381185] systemd-journald[115]: Received request to flush runtime journal from PID 1
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Load/Save Random Seed.
[ OK ] Started udev Coldplug all Devices.
[ OK ] Found device /dev/ttyS0.
Starting Create Volatile Files and Directories...
[ OK ] Started Create Volatile Files and Directories.
Starting Update UTMP about System Boot/Shutdown...
Starting Network Time Synchronization...
[ OK ] Started Network Time Synchronization.
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Reached target System Time Synchronized.
Starting Synchronize System and HW clocks...
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ 8.588595] EXT4-fs (mmcblk1p2): recovery complete
[ 8.594278] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ OK ] Reached target System Initialization.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on dropbear.socket.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 8.747607] FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
Starting Avahi mDNS/DNS-SD Stack...
Starting Permit User Sessions...
Starting Telephony service...
[ OK ] Started Kernel Logging Service.
Starting Login Service...
Starting uim-sysfs.service...
Starting Print notice about GPLv3 packages...
[ OK ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf.[ 8.986614] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
Starting Network Service...
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Started System Logging Service.
[ OK ] Started Permit User Sessions.
[ OK ] Started uim-sysfs.service.
[ OK ] Started Network Service.
[ 9.917060] net eth1: initializing cpsw version 1.15 (0)
[ 9.925064] net eth0: initialized cpsw ale version 1.4
[ 9.932722] net eth0: ALE Table size 1024
[ 10.035065] net eth1: phy found : id is : 0x221622 slave->phy->phy_id 2233890
[ 10.063768] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ 10.078876] net eth0: initializing cpsw version 1.15 (0)
[ 10.193965] net eth0: phy found : id is : 0x221622 slave->phy->phy_id 2233890
[ 10.221910] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ OK ] Started Telephony service.
[ OK ] Started Login Service.
[ OK ] Reached target Network.
Starting Lightning Fast Webserver With Light System Requirements...
Starting Network Name Resolution...
Starting rc.pvr.service...
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS0.
[ OK ] Reached target Login Prompts.
[ OK ] Started Lightning Fast Webserver With Light System Requirements.
[ OK ] Started Network Name Resolution.
[ 11.906753] random: nonblocking pool is initialized
[ OK ] Started rc.pvr.service.
Starting telnetd.service...
Starting tiipclad-daemon.service...
[ OK ] Started telnetd.service.
[ OK ] Started tiipclad-daemon.service.
Starting thttpd.service...
Starting my.service...
[ OK ] Started thttpd.service.
[ OK ] Started my.service.
Starting rng-tools.service...
[ OK ] Started rng-tools.service.
Starting thermal-zone-init.service...
[ OK ] Started thermal-zone-init.service.
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
binutils-dev
binutils
bison-dev
bison
cpp-symlinks
cpp
dosfstools
g++-symlinks
g++
gawk-dev
gawk
gcc-symlinks
gcc
gdb
gdbc6x
gdbserver
gstreamer1.0-libav
hidapi
libcairo-perf-utils
libgmp10
libidn11
libmpc3
libmpfr4
make
nettle
parted
swig-dev
swig
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org t ttyS0
Arago 2016.08 t ttyS0
t login:
lsmod 命令查看,一个驱动模块都未加载。设备接口都不可用。