This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 通过spi 外接 单色 sensor



dm368通过spi外接单色sensor实现拍照与视频的拍摄,然后保存,此功能能否实现?如果可以在davinci架构下有没有spi sensor 驱动代码可以参考

  • 你好,

    SPI是用来控制单色sensor的接口,还是单色sensor的数据也是从spi输出的?
  • 谢谢您的回答,spi是配置sensor寄存器的接口,sensor 数据输出采用的是10bit并行接口,而且sensor数据输出有帧行同步frame_valid line_valid
  • 你好,

    我能想到的问题是编码没有单色编码,都是支持的YUV格式。所以你是否能接受10bit只使用高8-bit作为亮度信息。然后在内存里先做一个0x8080的buffer作为UV信息。拼成一个YUV数据进行编码。

    采集的时候还需要配置为YUV8bit输入,直接ISIF存到DDR,不要过IPIPE,不做任何处理。
  • 您好,

    e2echina.ti.com/.../60205
    以上网页说MT9M034,他的输出有PIXCLK,DOUT[11:0]等,FV,LV信号,以968 rows of 1284 columns的方式输出,这样他可以直接和dm368的VPFE的PIXCLK,DOUT[11:0]相连,每个像素的数据可以不做处理,直接放置到内存中。

    以上可以实现的话,按道理我们的sensor( NOIP2SN1300A-QDI)也可以这样做的,麻烦看一下是否可以?还有你们Davinci下有没有spi接口的sensor驱动可以参考?先谢谢了