This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问下,如果要接收和压缩极大分辨率的图片,可以使用dm385吗,具体如何实现呢



分辨率比如13K*13K。dm385可以识别如此大分辨率的图片吗

  • 你好,

    请问接收通过什么接口?camera接口?帧率多少?ISIF并口可以接收13kx13k。下面的信息可以在数据手册里找到:

    Image Sensor Interface (ISIF) features:
    – Support for up to 32K pixels (image size) in both the horizontal and vertical direction

    但是JPEGenc最大支持16kx8k。

  • 这么大的图像,无法编码;
    ipnc rdk 3.5 最大 jpeg 编码为 4320 x 4320
    ipnc rdk 3.8 最大 jpeg 编码为 16384 x 8192