This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

高版本iar编译的StarterWare无法在SD卡运行

高版本iar 8.30编译StarterWareIAR现错误(Error[Lp049]: there was no reference to __iar_data_init3, but it is needed to initialize section .bss ....),修改了.icf文件 ,把 do not initialize  { section .noinit }; 改成了 do not initialize  { section .bss };(参考文章e2echina.ti.com/.../97888),消除编译报警。可以在线仿真,但是放到sd卡里无法运行!但是换成低版本7.20编译出来的都正常!请问这个问题如何解决?