This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 encode fps:0



dvsdk_2_10_01_18

dm368    Cores: ARM 432 MHz DDR:   340 MHz

root@192.168.0.60:/opt/dvsdk# ./loadmodules.sh

cmemk: no version for "struct_module" found: kernel tainted.

CMEMK module: built on Nov 27 2012 at 09:17:51

Reference Linux version 2.6.18   File /home/yq/dvsdk_2_10_01_18/linuxutils_2_24_02/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c

ioremap_nocache(0x85000000, 50331648)=0xc6000000

allocated heap buffer 0xc6000000 of size 0x134000

cmem initialized 20 pools between 0x85000000 and 0x88000000

CMEM Range Overlaps Kernel Physical - allowing overlap

 CMEM phys_start (0x1000) overlaps kernel (0x80000000 -> 0x84c00000)

ioremap_nocache(0x1000, 28672)=0xc5088000

 no remaining memory for heap, no heap created for memory block 1

cmem initialized 1 pools between 0x1000 and 0x8000

IRQK module: built on Nov 27 2012 at 09:20:41  

Reference Linux version 2.6.18   File /home/yq/dvsdk_2_10_01_18/linuxutils_2_24_02/packages/ti/sdo/linuxutils/irq/src/module/irqk.c irqk initialized EDMAK module: built on Nov 27 2012 at 09:20:40  

Reference Linux version 2.6.18   File /home/yq/dvsdk_2_10_01_18/linuxutils_2_24_02/packages/ti/sdo/linuxutils/edma/src/module/edmak.c

davinci_interrupt 354: VBUS error workaround (delay coming)

root@192.168.0.60:/opt/dvsdk# ./encode -v 2.264

Encode demo started.

vpfe ccdc capture vpfe ccdc capture.1: IMP chained

vpfe ccdc capture vpfe ccdc capture.1: Resizer present

MUX: initialized GPIO40

davinci_resizer davinci_resizer.2: RSZ_G_CONFIG:0:1:108

davinci_previewer davinci_previewer.2: ipipe_set_preview_config davinci_previewer

davinci_previewer.2: ipipe_set_preview_config

vpfe ccdc capture vpfe ccdc capture.1: IMP chained

vpfe ccdc capture vpfe ccdc capture.1: Resizer present

vpfe ccdc capture vpfe ccdc capture.1: hpitch = 720, vpitch = 480, bpp = 1

vpfe ccdc capture vpfe ccdc capture.1: hpitch = 720, vpitch = 480, bpp = 1

Starting ccdc_config_ycbcr...<7>

starting ccdc_reset...<7>

 End of ccdc_reset...<7>

Starting ccdc_setwin...<7>ipipe_set_resizer, resizer - A enabled

DavinciDisplay DavinciDisplay.1: Before finishing with S_FMT:

layer.pix_fmt.bytesperline = 736,  

layer.pix_fmt.width = 720, 

 layer.pix_fmt.height = 480,  

layer.pix_fmt.sizeimage =529920

 DavinciDisplay DavinciDisplay.1: pixfmt->width = 720,  layer->layer_info.config.line_length= 736

ARM Load: 0% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 0 kbps Time: 00:00:01 Demo: Encode Display: D1 NTSC Video Codec: H.264 HP Resolution: 720x480 Sound Codec: N/A Sampling Freq: N/A

ARM Load: 0% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 0 kbps Time: 00:00:02 Demo: Encode Display: D1 NTSC Video Codec: H.264 HP Resolution: 720x480 Sound Codec: N/A Sampling Freq: N/A

 

FPS一直0,求指点```