1、该EVM的摄像头数据接入是否都是通过Vision Application Board的FPD_LINK接入然后传入CPU Board?
2、激光雷达一般都是ETH接口,可以直接通过CPU Board的两个Gbit Eth接口接入吗?
3、Vision Application Board的CAN口是做什么用的?可否用于超声波雷达/毫米波雷达的数据接入?
4、CPU Borad的2个DCAN接口只能用于接header吗?是否支持车机控制信息的输出?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.