1. stk里面SRIO的descriptor定义的是64,看了其发送时对描述符的操作,实际是一个待应用协议扩展的host packet描述符,而srio协议扩展的字段仅2word(8 byte)对其到16边界应该为48,请问修改为48是否有其他的风险?
2. GE例程里描述符使用的标准不带扩展的8 word host packet描述符,其size为32,想将使用pa发送udp(主要进行udp/ip/eth层的checksum/crc自动生成和接收port至Queue的路由)没有找到此时描述符的格式,特请教其格式,疑惑仍然使用标准描述符即可?
另,如果能提供满足2需求的例程,特别是直接基于CSL的例子甚好。
致谢!