This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6416,焊接碰到难题,请指导

Other Parts Discussed in Thread: TMS320C6416

TI ,朋友们:

    我们之前买了1K TMS320C6416,因为屯放时间有点久,可能保管也有点不妥;现在有一些氧化问题。在我们贴片的时候,碰到有30%左右不良率。这不良产品中,有一部分卸下重新测试,芯片又好的,有一部分是坏了。现在有几个问题,看看是否能协助一下。

   现在我对焊接问题,提出下面请教,麻烦给以支持:

1,芯片焊接前烘烤的温度和时间要求?
2,芯片焊接的温度曲线要求?
3,芯片是否能反复按焊接曲线焊接?
4,芯片焊错需要重新植球是用铁板烧还是热风更适合?植球的温度要求?
5,含铅植球氧化后是否影响焊接质量?
6,芯片是否可以浸泡在酒精中用超声波清洗?

谢谢