This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm6446 vpfe 与fpga连接,无法capture正确的图像数据

hi,

 自己的设计的开发板,使用dm6446芯片,没有使用AD芯片,输入直接从fpga接dsp 的vpfe,bt656的格式,fpga的数据pin0-pin7 连接vpfe的ccd0-ccd7,clk连接vpfe的pclk,现在的问题是,我直接使用ti提供的demo,vga_loop,屏蔽初始化ad函数无法capture到fpga的输入过来的数据。

fpga的输入数据和时钟都已经用示波器测试确定都正确,请问我还需要设置什么呢?

我的vpfe配置如下:

void vpfe_init( Uint32 buffer, Uint32 width, Uint32 height,Uint8 channel )
{

    VPFE_SYN_MODE   = 0x00032F87;   // interlaced, with VD pority as negative
    VPFE_HD_VD_WID  = 0;
 VPFE_PIX_LINES  = 0;  //linger 720x624
    /*
     *  sph = 1, nph = 1440, according to page 32-33 of the CCDC spec
     *  for BT.656 mode, this setting captures only the 720x480 of the
     *  active NTSV video window
     */
    VPFE_HORZ_INFO  = width << 1;   // Horizontal lines
    VPFE_HSIZE_OFF  = width << 1;   // Horizontal line offset
    VPFE_VERT_START = 0;            // Vertical start line
    VPFE_VERT_LINES = height >> 1;  // Vertical lines
    VPFE_CULLING    = 0xFFFF00FF;   // Disable cullng

    /*
     *  Interleave the two fields
     */
    VPFE_SDOFST     = 0x00000249;
    VPFE_SDR_ADDR   = buffer;
    VPFE_CLAMP      = 0;
    VPFE_DCSUB      = 0;
    VPFE_COLPTN     = 0xEE44EE44;
    VPFE_BLKCMP     = 0;
    VPFE_FPC_ADDR   = 0x86800000;
    VPFE_FPC        = 0;
    VPFE_VDINT      = 0;
    VPFE_ALAW       = 0;
    VPFE_REC656IF   = 0x00000003;
    /*
     *  Input format is Cb:Y:Cr:Y, w/ Y in odd-pixel position
     */
 VPFE_CCDCFG     = 0x00008800;//800
 VPFE_FMTCFG     = 0x00008000;  //linger//0
    VPFE_FMT_HORZ   = 0x000002D0;
    VPFE_FMT_VERT   = 0x00000240;//0x00000272;
    VPFE_FMT_ADDR0  = 0;
    VPFE_FMT_ADDR1  = 0;
    VPFE_FMT_ADDR2  = 0;
    VPFE_FMT_ADDR3  = 0;
    VPFE_FMT_ADDR4  = 0;
    VPFE_FMT_ADDR5  = 0;
    VPFE_FMT_ADDR6  = 0;
    VPFE_FMT_ADDR7  = 0;
    VPFE_PRGEVEN_0  = 0;
    VPFE_PRGEVEN_1  = 0;
    VPFE_PRGODD_0   = 0;
    VPFE_PRGODD_1   = 0;
    VPFE_VP_OUT     = 0x04E22D00;//41a2d00
    VPFE_PCR        = 0x00000001;   // Enable CCDC
}