AM335X开发包中是否有对PS2键盘的支持?如果没有,请问有什么方法可以支持PS2?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
没有支持,需要转接芯片,然后找到对应的驱动,我们暂时没有这方面的经验,因为现在没人用这个口了
请问,我接了转接芯片WIT122UHM,需要对应那些驱动呢?网络上查到的结果说这个PS2的转接芯片是免驱动啊!!!!
驱动您需要和转接芯片供应商联系了,免驱是指在什么os的什么版本里免驱,是否需要配置这个驱动
我用的也是AM3354的芯片,USB口接的是USB2514芯片作为USB HUB,然后,在hub中引出一组D3+ 、D3-信号接到PS/2模块的WIT122UH芯片上,这种接法的话,USB驱动应该会把PS/2键盘当做USB键盘来识别吧?需要在linux内核做其他的配置吗?
我用的也是AM3354的芯片,USB口接的是USB2514芯片作为USB HUB,然后,在hub中引出一组D3+ 、D3-信号接到PS/2模块的WIT122UH芯片上,这种接法的话,USB驱动应该会把PS/2键盘当做USB键盘来识别吧?需要在linux内核做其他的配置吗?
这里免驱有两种,一种是对于AM335x来说,转接芯片是透明的,硬件自己做的转换,对于这样的情况,只要配置usb 鼠标就可以了。
另一种,对于AM335x来说,这个是芯片是需要配置的,如果这样,那么需要有机遇usb的驱动进行配置,这个驱动应该来自于桥接芯片供应商。
因此,您可以拿个一般的usb鼠标试试,如果usb鼠标可以用,但是转接了ps2的不能用,那么就说明芯片需要配置。