This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368 vpfe sensor

硬件:dm368 通过vpfe外接 sensor,此sensor 与dm368连接有10bit 数据线,bayer格式的raw数据输入

请问一下,sensor--->isif----->ddr,保存raw数据到ddr内,保存数据是10bit还是8bit?或者16bit?

isif 可以把10bit压缩为8bit吗?

看官方evm板,dm368外接mt9p031 sensor(12bit),ddr保存的raw数据是16bit

  • user4346463 说:
    请问一下,sensor--->isif----->ddr,保存raw数据到ddr内,保存数据是10bit还是8bit?或者16bit?

    硬件连接最低10bit,输出可以是10bit,或者是压缩的8-bit,软件可以配置。

    user4346463 说:
    看官方evm板,dm368外接mt9p031 sensor(12bit),ddr保存的raw数据是16bit

    超过8-bit的数据,在内存存放要占用两个字节,也就是16 bit。

  • 再请问一下,如果10bit压缩为8bit时,是用最高位8bit,然后最低2bit截掉?还是用什么算法进行压缩?isif硬件压缩的吗?