This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678烧写问题求助



现在在进行6657和6678的开发,想向Ti的工程师求助。

66x系列的芯片是否具有使用串口远程烧写更新程序的功能?以前用过的6748,可以在PC端通过串口烧写AIS文件到板上的FLASH,从而更新程序。

现在请问66系列的芯片,是否具有这样的功能,是否有相应的串口烧写工具和例程提供?

谢谢!

  • 没有这样的串口烧写工具和例程,c66x bootloader和C674x不一样,不是AIS格式,代码是转换成boot table的。如果想要做远程更新代码的话,可以先通过uart boot mode从主机端加载并运行烧写程序,新的代码由这个烧写程序通过串口读取并烧写到flash。