This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678设计问题,PCIE,SRIO时钟问题



6678开发板,SRIO时钟312.5M,研读手册发现,312M的时钟也可以换成别的,经过PLL后可以实现1.25,2.5,3.125,5这四种数据率,可以这么理解吧!在我的设计里V6 FPGA 的GTX与6678SRIO直连,在6678的收端RX放置0.1uF电容,FPGA的RX端放置0.1UF电容,那么FPGA端的GTX时钟需要跟DSP的SRIO时钟同源吗?比如,用同一个312.5M时钟经过一个双路驱动给SRIO和GTX提供时钟,需要吗?

6678 PCIE也与V6 FPGA GTX直连,电容放置方法SRIO, 手册上说,PCIE link的两端时钟最好使用同一个参考时钟,但又提到不使用同一个时钟也可以,需要做相应的设置,这块不太肯定,工程师给看看,需要FPGA的PCIE时钟需要和6678的PCIE时钟是同一个时钟吗