This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教下关于QMSS的descriptor问题



1. 描述符的对齐字节,看stk里面mono和host分别的对其是64/128,翻阅手册并未发现哪里有描述;那么 对host buffer是否同样有对齐要求呢?

2. stk里面SRIO的descriptor定义的是64,看了其发送时对描述符的操作,实际是一个应用协议扩展的host packet描述符,而srio协议扩展的字段仅2word(8 byte)对其到16边界应该为48,请问实际使用64仅仅是额外的padding还是有其他作用,比如pktdma处理的时候或填充额外的信息?

3. GE stk例程里描述符使用的标准不带扩展的8 word host packet描述符,其size为32,想将使用pa发送udp(主要进行udp/ip/eth层的checksum/crc自动生成和接收port至Queue的路由)没有找到此时描述符的格式,特请教其格式,抑或其仍然使用标准描述符即可?仅仅pa的cmd配置描述符因为额外的配置信息的承载,需要128(这个倒是有明确描述:实际命令最大使用112,添加额外的16padding)。

望ti专家及各路专家解答,感谢!