在CCS4.2环境中,使用XDS100V2 jTAG emulation 连接OMAP L138中ARM,出现如下 错误
Error connecting to the target:
Error 0x80002240/-180
Fatal Error during: Initialization, OCS, Control,
请各位专家帮助解释一下,谢谢先。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在CCS4.2环境中,使用XDS100V2 jTAG emulation 连接OMAP L138中ARM,出现如下 错误
Error connecting to the target:
Error 0x80002240/-180
Fatal Error during: Initialization, OCS, Control,
请各位专家帮助解释一下,谢谢先。
CCS连不上,如下检查:
1、XDS100v2驱动能力很一般,所以线缆到omapl138不能距离太长。
2、omapl138的boot模式,是否是仿真状态?emulation状态。注意拨码方式,仔细阅读一下guide。
3、你是否有TI原装开发板OMAP-L138开发板,开发板把xds100这部分电路坐进去了。你直接用usb口连电脑,就可以的。ccs4里有驱动。和开发板对比一下。
4、你仔细按照这个页面的描述,检查一下,一定可以连上的。
processors.wiki.ti.com/.../AM1808_EVM_board_using_CCS%3F
5、我的QQ号是:315676522,有问题可一起讨论。