传输模式:am5728采用标准RS422接口形式传输压缩后的图像数据和视频数据,有效输出数据码率不大于3.2Mbps。
通讯接口:同步RS422
通信速率:3.2 Mbps和1.8Mbps可切换(默认3.2Mbps)
传输方向:am5728到数据终端
数据内容:H.264编码图像数据;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
下面建议请参考:
首先需要实现RS422,请参考:
然后,你需要在软件上给码流添加一个header,里面包含码流开始的标志,码流长度等信息,在接收端通过这些信息来找到码流开始的地方,已经码流长度。