This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138 nor-flash-write运行出错

Other Parts Discussed in Thread: OMAP-L138

通过TI所提供的nor-flashwrite对OMAPL138的nor flash进行读写,当通过XDS100V2和CCS4.2连接后,在ARM中导入norflash-write.out后运行,出现以下错误,请各位专家帮助看看。 (ps: norflash-write.out是TI DVSDK中提供的Image文件。)

Starting DA850/OMAP-L138 NOR Flash Writer.

DA850/OMAP-L138 part detected.

Its an ARM boot device You require two images to boot this device 1) ARM UBL in AIS file format. 2) U-Boot image in raw binary format To generate the AIS format file, you need to run the ARM/DSP .out (COFF) file generated from CCS build through the AISGen tool.

CFI Query...failed.

ERROR: NOR Initialization failed. NOR flashing failed!