This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6713B的BOOTMOD和HPI管脚冲突问题



C6713B的启动模式是通过复位的时候采集HPI数据管脚HD4~3内容设置的,通过对这两根线连接上拉、下拉电阻可以选择启动是从HPI还是从外部ROM。

我的疑问是这个上下拉电阻是否会影响正常HPI接口工作时HD4,HD3的数值? 

我看了6713dsk的原理图,上下拉电阻是通过switch连到这两根数据线上,我的理解是启动的时候switch选择导通让上下拉电阻生效,启动后手动拨动switch让其断开,这样的确是可以不影响正常的HPI工作。但是对于产品设计,每次使用的时候去手动拨动switch是不现实的。

请问一下我的理解是否正确?产品设计的时候如何解决Bootmod和HPI数据线冲突的问题?

  • 这个上下拉电阻不会影响正常HPI接口工作时HD4,HD3的数值,这个switch是让HD4, HD3输出不同的高低电平来选择相应的boot mode,只有在器件Reset时,HD4, HD3作为boot mode管脚,Reset后就是HPI功能管脚。