This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS32C6671的技术问题



1.DSP6671 作为PCIE的RC,PowerPC作为EP,直连无SWITCH,使用DSP的官方PCIE测试程序,可以读取到0x21802000为PowerPC的VENDOR和DEVICE号,DSP配置outbound后(0x21802010为0x0000000)读取BAR0对应的0x60000000地址没有得到正确的数据(读为0),,

  这个问题已解决,原因是未使能command中的mem位

2.DSP6671作为PCIE的RC,接一级PCIE SWITCH后再接一级PCIE2PCI桥片,再接2个DSP6455,目前可以枚举PCIE SWITCH,无法枚举到PCIE2PCI桥,更无法枚举到2个6455,请问要如何才能枚举成功?  枚举成功的依据为0x21802000有相应的VENDOR和DEVICE号, 使用DSP的官方PCIE测试程序的。请问:PCIE SWITCH的枚举算法怎么实现?下游端口的状态信息如何获取?SWITCH桥片为PEX 8604。谢谢解答!

  • 您好:

        在使用DPS6671的时候,遇到两个问题需要请教一下:

        1.DSP6671 作为PCIE的RC,PowerPC作为EP,直连无SWITCH,使用DSP的官方PCIE测试程序,可以读取到0x21802000为PowerPC的VENDOR和DEVICE号,DSP配置outbound后(0x21802010为0x0000000)读取BAR0对应的0x60000000地址没有得到正确的数据(读为0),请问该如何处理呀?

        2.DSP6671作为PCIE的RC,接一级PCIE SWITCH后再接一级PCIE2PCI桥片,再接2个DSP6455,目前可以枚举PCIE SWITCH,无法枚举到PCIE2PCI桥,更无法枚举到2个6455,请问要如何才能枚举成功?  枚举成功的依据为0x21802000有相应的VENDOR和DEVICE号, 使用DSP的官方PCIE测试程序的。