This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESD测试时引发的H3A模块数据混乱问题

我们在做ESD测试时,发现M3VPSS的ISS子系统,H3A模块中的数据(fullH3ABufAddr)会因静电而变的不正常。这个数据我们会用来计算sensor曝光时间和增益。它被静电打坏之后会导致曝光时间和增益计算错误,从而导致图像变暗或者变亮。在这个结构体中,错误的数据字段我用注释标注出来啦:

typedef struct
{
    Task_Handle taskHndl;
    Semaphore_Handle sem;

    FVID2_Handle SensorHandle;
    FVID2_Handle cameraVipHandle;

    AEWB_VENDOR aewbVendor;
    UInt32      aewbMode;
        UInt32                aewbModeFlag;
    UInt32      aewbPriority;

    MSP_IspH3aCfgT           ispH3aCfg;
    MSP_IspConfigProcessingT *pIssConfig;
    MSP_COMPONENT_TYPE       *pIspHandle;
    Void                     *pAlgHndl;

    UInt32 h3aBufAddr[2];
    UInt32 fullH3ABufAddr; //就是这个数据不正常!
    UInt32 curH3aBufIdx;
    UInt32 h3aBufSize;
    Void   *pH3AMem;

    UInt32 aewbNumWinH;
    UInt32 aewbNumWinV;
    UInt32 aewbNumPix;

    volatile UInt32 exitFlag;

    Int32 AutoIris;
    Int32 saturation;
    Int32 sharpness;
    Int32 brightness;
    Int32 contrast;
    Int32 blc;
    Int32 AWBMode;
    Int32 AEMode;
    Int32 Env;
    Int32 Binning;
    Int32 FrameRate;

    UInt8  *dcc_Default_Param;
    Int32  dcc_init_done;
    UInt32 dccSize;
    UInt32 AFValue;
    UInt32 AEWBValue1;
    UInt32 AEWBValue2;
}Iss_2AObj;

我发现H3A模块的H3A_PCR寄存器中有一个OVF位可以检测overflow,但是似乎没起作用,图像变暗或者变亮之后检测这个位始终是0。


有大佬知道这个怎么解决吗?