This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

可否将AM3358的EMIF16接口拆分成2个8bit 一个实现DDR2、一个接NAND FLASH 或FPGA

Other Parts Discussed in Thread: AM3358

AM3358的EMIF16可以实现2个8bit;

但是否可以

1)一个8bit接DDR2/3,另一个8bit接FPGA;控制信号、地址信号怎么办,需要复用了,DDR2/3需要短接,FPGA不容易各种要求;

2)16bit可否将DDR2/3和FPGA级联起来;同时接这两个设备?

3)AM3358实现GbE等高速外设时,是否需要挂载DDR?,即要挂载DDR又要实现FPGA并行通信怎么办