This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UBI image Failed to switch_root, dropping to a shell why?

Other Parts Discussed in Thread: DM3730

I am making a UBI image to boot our board DM3730.
 mkfs.ubifs -r -F /home/bradlee/targetfs/rootfs -m 2048 -e 129024 -c 3996 -o ubifs.img
 ubinize -o ubi.img -m 2048 -p 128KiB -s 512 -O 512 ubinize.cfg
 results:
[   29.877014] UBI: attaching mtd4 to ubi0
[   29.880859] UBI: physical eraseblock size:   131072 bytes (128 KiB)
[   29.887207] UBI: logical eraseblock size:    129024 bytes
[   29.892669] UBI: smallest flash I/O unit:    2048
[   29.897369] UBI: sub-page size:              512
[   29.902038] UBI: VID header offset:          512 (aligned 512)
[   29.907897] UBI: data offset:                2048
[   30.848876] UBI: attached mtd4 to ubi0
[   30.852722] UBI: MTD device name:            "File System"
[   30.858215] UBI: MTD device size:            499 MiB
[   30.863220] UBI: number of good PEBs:        3996
[   30.867980] UBI: number of bad PEBs:         0
[   30.872436] UBI: max. allowed volumes:       128
[   30.877075] UBI: wear-leveling threshold:    4096
[   30.881805] UBI: number of internal volumes: 1
[   30.886291] UBI: number of user volumes:     1
[   30.890777] UBI: available PEBs:             0
[   30.895233] UBI: total number of reserved PEBs: 3996
[   30.900238] UBI: number of PEBs reserved for bad PEB handling: 39
[   30.906372] UBI: max/mean erase counter: 1/0
[   30.910644] UBI: image sequence number: 393079821
[   30.915405] UBI: background thread "ubi_bgt0d" started, PID 572
UBI device number 0, total 3996 LEBs (515579904 bytes, 491.7 MiB), available 0 LEBs (0 bytes), LEB size 129024 bytes (126.0 KiB)
[   30.959197] UBIFS: recovery needed
[   31.031616] UBIFS: recovery completed
[   31.035308] UBIFS: mounted UBI device 0, volume 0, name "rootfs"
[   31.041381] UBIFS: file system size:   508612608 bytes (496692 KiB, 485 MiB, 3942 LEBs)
[   31.049438] UBIFS: journal size:       9033728 bytes (8822 KiB, 8 MiB, 71 LEBs)
[   31.056793] UBIFS: media format:       w4/r0 (latest is w4/r0)
[   31.062652] UBIFS: default compressor: lzo
[   31.066772] UBIFS: reserved for root:  0 bytes (0 KiB)
Failed to switch_root, dropping to a shell


 
ubinize.cfg list below:
[ubifs]
mode=ubi
image=ubifs.img
vol_id=0
vol_size=450MiB
vol_type=dynamic
vol_alignment=1
vol_name=rootfs
vol_flags=autoresize
then I burn the image using following command:
/burn_flash.sh 192.168.0.13

burn_flash.sh is list below:
#!/bin/sh

echo tftp server ipaddr is $1
tftp -gr rootfs.ubi $1
umount /newroot
ubidetach /dev/ubi_ctrl -m 4
flash_erase /dev/mtd4 0 0
#ubiformat -y /dev/mtd4 -f rootfs.ubi
ubiformat /dev/mtd4 -f rootfs.ubi
ubiattach /dev/ubi_ctrl -m 4
mount -t ubifs ubi0:rootfs /newroot

init
!/bin/sh
echo "Start initramfs from /init"

mount -t proc proc /proc
mount -t sysfs sysfs /sys

#echo 0 > /proc/sys/kernel/printk

#clear

busybox --install -s
mkdir -p /dev/
#mknod /dev/null c 1 3
#mknod /dev/tty c 5 0
#mknod /dev/console c 5 1
mdev -s

get_opt() {
    echo "$@" | cut -d "=" -f 2
}

init="/sbin/init"
#root="/opt/test1/buildroot-2011.11/output/target"

for i in $(cat /proc/cmdline); do
    case $i in
        root\=*)
            root=$(get_opt $i)
            ;;
        init\=*)
            init=$(get_opt $i)
            ;;
    esac
done

echo "root=$root init=$init"

echo "Mount..."
#mount -t nfs -o nolock 192.168.1.1:"${root}" /newroot
mkdir -p /newroot
ubiattach /dev/ubi_ctrl -m 4
mount -t ubifs ubi0:rootfs /newroot

if [[ -x "/newroot/${init}" ]] ; then
    umount /sys /proc
    exec switch_root /newroot "${init}"
fi

echo "Failed to switch_root, dropping to a shell"
#exec sh
exec /sbin/init