This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6457的EDMA无法重复发送问题

C6457板子承载SYS/BIOS系统,采用McBSP + EMDA方式进行回环测试, 调试运行可是一次数据收发,可是无法实现第二次乃至多次数据收发测试,无法进入中断处理函数。

1、通道PaRam参数已经在第一次数据完成收发时进行更新(通过查看寄存器与第一次参数一致)

2、通过查看寄存器,事件使能寄存器EER/EERH,事件中断寄存器IER/IERH都正常;

3、通过查看McBSP数据DDR、DXR,发现数据没有更新为第二次发送的数据;

4、通过自动重载参数方式,也不可行,不知道哪里出的问题。。。。

请问下,还缺少什么设置?   提供的例子全是只有一次发送的, 没有多次发送的,一脸迷茫。