This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIC23采集声音过小如何调整



我用的板子是5509A的,在进行实时采集回放时,只有对着麦克风口才有输出,那我要离麦克风远一点采集的话应该修改哪一段程序呢?

#include <csl.h>
#include <csl_i2c.h>
#include <stdio.h>
#include <csl_pll.h>
#include <csl_mcbsp.h>
#define CODEC_ADDR 0x1A
/*锁相环的设置*/
PLL_Config  myConfig      = {
  0,    //IAI: the PLL locks using the same process that was underway
                //before the idle mode was entered
  1,    //IOB: If the PLL indicates a break in the phase lock,
                //it switches to its bypass mode and restarts the PLL phase-locking
                //sequence
  24,    //PLL multiply value; multiply 24 times
  1             //Divide by 2 PLL divide value; it can be either PLL divide value
                //(when PLL is enabled), or Bypass-mode divide value
                //(PLL in bypass mode, if PLL multiply value is set to 1)
};
MCBSP_Config Mcbsptest;
/*设置McBSP,使用McBSP1来发送和接收来自DSP 和 AIC23的数据*/
/*McBSP set,we use mcbsp1 to send and recieve the data between DSP and AIC23*/
MCBSP_Config Mcbsp1Config = {
MCBSP_SPCR1_RMK(
MCBSP_SPCR1_DLB_OFF,                   /* DLB    = 0,禁止数字回环方式 */
MCBSP_SPCR1_RJUST_LZF,                 /* RJUST  = 2 接收数据符号扩展和调节方式*/
MCBSP_SPCR1_CLKSTP_DISABLE,            /* CLKSTP = 0 */
MCBSP_SPCR1_DXENA_ON,                  /* DXENA  = 1 DX引脚延时使能打开*/
0,                                     /* ABIS   = 0 */
MCBSP_SPCR1_RINTM_RRDY,                /* RINTM  = 0 接收中断模式*/
0,                                     /* RSYNCER = 0 接收帧同步错误标志*/
MCBSP_SPCR1_RRST_DISABLE               /* RRST   = 0 禁止接收器复位*/
),
    MCBSP_SPCR2_RMK(
    MCBSP_SPCR2_FREE_NO,                   /* FREE   = 0 */
    MCBSP_SPCR2_SOFT_NO,                   /* SOFT   = 0 */
    MCBSP_SPCR2_FRST_FSG,                  /* FRST   = 0 帧同步逻辑复位 */
    MCBSP_SPCR2_GRST_CLKG,                 /* GRST   = 0 采样率发生器复位 */
    MCBSP_SPCR2_XINTM_XRDY,                /* XINTM  = 0 发送中断模式*/
    0,                                     /* XSYNCER = N/A */
    MCBSP_SPCR2_XRST_DISABLE               /* XRST   = 0 发送器复位*/
   ),
   /*单数据相,接受数据长度为16位,每相2个数据*/
  MCBSP_RCR1_RMK(
          MCBSP_RCR1_RFRLEN1_OF(1),              /* RFRLEN1 = 1 接收阶段1的帧长为1个字 */
          MCBSP_RCR1_RWDLEN1_16BIT               /* RWDLEN1 = 2 接收阶段1的字长为16位 */
  ),
  MCBSP_RCR2_RMK(
    MCBSP_RCR2_RPHASE_SINGLE,              /* RPHASE  = 0 接收帧的阶段数*/
    MCBSP_RCR2_RFRLEN2_OF(0),              /* RFRLEN2 = 0 接收阶段2关闭*/
    MCBSP_RCR2_RWDLEN2_8BIT,               /* RWDLEN2 = 0 接收阶段2的字长为8位*/
    MCBSP_RCR2_RCOMPAND_MSB,               /* RCOMPAND = 0 接收数据压扩模式*/
    MCBSP_RCR2_RFIG_YES,                   /* RFIG    = 0  忽略不期望接收的帧同步信号 */
    MCBSP_RCR2_RDATDLY_1BIT                /* RDATDLY = 1 接收数据延时*/
    ),
   MCBSP_XCR1_RMK(
    MCBSP_XCR1_XFRLEN1_OF(1),              /* XFRLEN1 = 1 发送阶段1的帧长(一个)*/
    MCBSP_XCR1_XWDLEN1_16BIT               /* XWDLEN1 = 2 发送阶段1的字长16位*/
),
MCBSP_XCR2_RMK(
    MCBSP_XCR2_XPHASE_SINGLE,              /* XPHASE  = 0 */
    MCBSP_XCR2_XFRLEN2_OF(0),              /* XFRLEN2 = 0 */
    MCBSP_XCR2_XWDLEN2_8BIT,               /* XWDLEN2 = 0 */
    MCBSP_XCR2_XCOMPAND_MSB,               /* XCOMPAND = 0 */
    MCBSP_XCR2_XFIG_YES,                   /* XFIG    = 0 */
    MCBSP_XCR2_XDATDLY_1BIT                /* XDATDLY = 1 发送数据延时*/
  ),
MCBSP_SRGR1_DEFAULT,
MCBSP_SRGR2_DEFAULT,
MCBSP_MCR1_DEFAULT,
MCBSP_MCR2_DEFAULT,
MCBSP_PCR_RMK(
   MCBSP_PCR_IDLEEN_RESET,                 /* IDLEEN   = 0   */
   MCBSP_PCR_XIOEN_SP,                     /* XIOEN    = 0   */
   MCBSP_PCR_RIOEN_SP,                     /* RIOEN    = 0   */
   MCBSP_PCR_FSXM_EXTERNAL,                /* FSXM     = 0   */
   MCBSP_PCR_FSRM_EXTERNAL,                /* FSRM     = 0   */
   0,                                      /* DXSTAT = N/A   */
   MCBSP_PCR_CLKXM_INPUT,                  /* CLKXM    = 0   */
   MCBSP_PCR_CLKRM_INPUT,                  /* CLKRM    = 0   */
   MCBSP_PCR_SCLKME_NO,                    /* SCLKME   = 0   */
   MCBSP_PCR_FSXP_ACTIVEHIGH,              /* FSXP     = 0   */
   MCBSP_PCR_FSRP_ACTIVEHIGH,              /* FSRP     = 1   */
   MCBSP_PCR_CLKXP_FALLING,                /* CLKXP    = 1   */
   MCBSP_PCR_CLKRP_RISING                  /* CLKRP    = 1   */
),
MCBSP_RCERA_DEFAULT,
MCBSP_RCERB_DEFAULT,
MCBSP_RCERC_DEFAULT,
MCBSP_RCERD_DEFAULT,
MCBSP_RCERE_DEFAULT,
MCBSP_RCERF_DEFAULT,
MCBSP_RCERG_DEFAULT,
MCBSP_RCERH_DEFAULT,
MCBSP_XCERA_DEFAULT,
MCBSP_XCERB_DEFAULT,
MCBSP_XCERC_DEFAULT,
MCBSP_XCERD_DEFAULT,
MCBSP_XCERE_DEFAULT,
MCBSP_XCERF_DEFAULT,
MCBSP_XCERG_DEFAULT,
MCBSP_XCERH_DEFAULT
};
/*创建和初始化I2C模块*/
/* This next struct shows how to use the I2C API */
/* Create and initialize an I2C initialization structure */
I2C_Setup I2Cinit = {
        0,              /* 7 bit address mode */
        0,         /* own address - don't care if master */
        84,            /* clkout value (Mhz)  */
        50,            /* a number between 10 and 400*/
        0,              /* number of bits/byte to be received or transmitted (8)*/
        0,              /* DLB mode on*/
        1               /* FREE mode of operation on*/
};
I2C_Config testI2C;
/*数字音频接口格式设置
AIC23为主模式,数据为DSP模式,数据长度16位*/
Uint16 digital_audio_inteface_format[2]={0x0e,0x53};
/*AIC23的波特率设置,采样率为44.1K*/
Uint16 sample_rate_control[2] = {0x10,0x23};
/*AIC23寄存器复位*/
Uint16 reset[2] ={0x1e,0x00};
/*AIC23节电方式设置,所有部分均所与工作状态*/
Uint16 power_down_control[2] ={0x0c,0x01};
/*AIC23模拟音频的控制
DAC使能,ADC输入选择为Line*/
Uint16 analog_aduio_path_control[2] ={0x08,0x14};
/*AIC23数字音频通路的控制*/
Uint16 digital_audio_path_control[2] ={0x0a,0x05};
/*AIC23数字接口的使能*/
Uint16 digital_interface_activation[2] ={0x12,0x01};
/*AIC23左通路音频调节*/
Uint16 left_line_input_volume_control[2] ={0x00,0x17};
/*AIC23右通路音频调节*/
Uint16 right_line_input_volume_control[2] ={0x02,0x17};
/*AIC23耳机左通路音频调节*/
Uint16 left_headphone_volume_control[2] ={0x05,0xFF};
/*AIC23耳机右通路音频调节*/
Uint16 right_headphone_volume_control[2] = {0x07,0xFF};
/*定义McBSP的句柄*/
MCBSP_Handle hMcbsp;
Uint16 i2c_status;
Uint16 i,temp;
void delay(Uint32 k)
{
   while(k--);
}
void main(void)
{
    Uint16 aic23data = 0;
        i2c_status = 1;
    /* Initialize CSL library - This is REQUIRED !!! */
    /*初始化CSL库*/
    CSL_init();
        /*设系统的运行速度为140MHz*/
    PLL_config(&myConfig);
    /* Initialize I2C, using parameters in init structure */
    /*初始化I2C的格式*/
//        I2C_config(&Config);
//        I2C_start();
//        I2C_getConfig(&Config1);
        /*I2C is undet reset*/
        I2C_RSET(I2CMDR,0);
        /*设置预分频寄存器,I2C的mode clock is 10MHz*/
        delay(100);
        I2C_RSET(I2CSAR,0x001A);
        I2C_RSET(I2CMDR,0x0620);
    I2C_setup(&I2Cinit);
          /*设置I2C的Mater clock*/
        I2C_RSET(I2CCLKL,100);
        I2C_RSET(I2CCLKH,100);
    I2C_getConfig(&testI2C);
        /*初始化McBSP0*/
        hMcbsp = MCBSP_open(MCBSP_PORT1,MCBSP_OPEN_RESET);
        /*设置McBSP0*/
        MCBSP_config(hMcbsp,&Mcbsp1Config);
        /*启动McBSP0*/
        MCBSP_start(hMcbsp,
                MCBSP_RCV_START | MCBSP_XMIT_START,
                0);
    MCBSP_getConfig(hMcbsp,&Mcbsptest);
    /*reset AIC23*/
    i2c_status = I2C_write( reset,          //pointer to data array  指向发送数据的数组
                                    2,                                //length of data to be transmitted  发送数据的长度16位
                                    1,                                //master or slaver   主模式
                                    CODEC_ADDR,            //slave address to transmit to 从地址发送
                                    1,                                //transfer mode of operation 传输模式
                                    30000                        //time out for bus busy    延时
                                        );
        delay(1000);
    /*设置AIC23各部分均工作*/
    i2c_status = I2C_write( power_down_control,//pointer to data array    省电控制
                                    2,                                //length of data to be transmitted
                                    1,                                //master or slaver
                                    CODEC_ADDR,            //slave address to transmit to
                                    1,                                //transfer mode of operation
                                    30000                        //time out for bus busy
                                        );
        /*设置AIC23的数字接口*/
        i2c_status = I2C_write( digital_audio_inteface_format,//pointer to data array 数字音频格式
                                    2,                                //length of data to be transmitted
                                    1,                                //master or slaver
                                    CODEC_ADDR,            //slave address to transmit to
                                    1,                                //transfer mode of operation
                                    30000                        //time out for bus busy
                                           );
         /*设置AIC23模拟通路*/
        i2c_status = I2C_write( analog_aduio_path_control,//pointer to data array  模拟音频格式
                                    2,                                //length of data to be transmitted
                                    1,                                //master or slaver
                                    CODEC_ADDR,            //slave address to transmit to
                                    1,                                //transfer mode of operation
                                    30000                        //time out for bus busy
                                        );
        /*设置数字通路*/
        i2c_status = I2C_write( digital_audio_path_control,//pointer to data array 数字音频通路控制
                                    2,                                //length of data to be transmitted
                                    1,                                //master or slaver
                                    CODEC_ADDR,            //slave address to transmit to
                                    1,                                //transfer mode of operation
                                    30000                        //time out for bus busy
                                          );
        /*设置AIC23的采样率*/
        i2c_status = I2C_write( sample_rate_control,//pointer to data array     采样速率
                                    2,                                //length of data to be transmitted
                                    1,                                //master or slaver
                                    CODEC_ADDR,            //slave address to transmit to
                                    1,                                //transfer mode of operation
                                    30000                        //time out for bus busy
                                    );
        /*设置耳机音量*/
        i2c_status = I2C_write( left_headphone_volume_control,//pointer to data array 耳机左声道音量调节
                                    2,                                //length of data to be transmitted
                                    1,                                //master or slaver
                                    CODEC_ADDR,            //slave address to transmit to
                                    1,                                //transfer mode of operation
                                    30000                        //time out for bus busy
                                    );
        i2c_status = I2C_write( right_headphone_volume_control,//pointer to data array  耳机右声道音量调节
                                    2,                                //length of data to be transmitted
                                    1,                                //master or slaver
                                    CODEC_ADDR,            //slave address to transmit to
                                    1,                                //transfer mode of operation
                                    30000                        //time out for bus busy
                                    );
        /*设置Line输入的音量*/
        i2c_status = I2C_write( left_line_input_volume_control,//pointer to data array  左声道音量调节
                                    2,                                //length of data to be transmitted
                                    1,                                //master or slaver
                                    CODEC_ADDR,            //slave address to transmit to
                                    1,                                //transfer mode of operation
                                    30000                        //time out for bus busy
                                    );
        i2c_status = I2C_write( right_line_input_volume_control,//pointer to data array  右声道音量调节
                                    2,                                //length of data to be transmitted
                                    1,                                //master or slaver
                                    CODEC_ADDR,            //slave address to transmit to
                                    1,                                //transfer mode of operation
                                    30000                        //time out for bus busy
                                    );
        /*启动AIC23*/
        i2c_status = I2C_write( digital_interface_activation,//pointer to data array  数字接口激活
                       2,                                //length of data to be transmitted
                       1,                                //master or slaver
                       CODEC_ADDR,            //slave address to transmit to
                       1,                                //transfer mode of operation
                       30000                        //time out for bus busy
                       );
        /*回放音频*/
        while(TRUE)
        {
                while(!MCBSP_rrdy(hMcbsp)){};
                aic23data = MCBSP_read16(hMcbsp);
                MCBSP_write16(hMcbsp,aic23data);
            }
}
  • 要修改AIC23寄存器配置,具体改什么值建议到音频论坛咨询。
    /*AIC23左通路音频调节*/
    Uint16 left_line_input_volume_control[2] ={0x00,0x17};
    /*AIC23右通路音频调节*/
    Uint16 right_line_input_volume_control[2] ={0x02,0x17};
    /*AIC23耳机左通路音频调节*/
    Uint16 left_headphone_volume_control[2] ={0x05,0xFF};
    /*AIC23耳机右通路音频调节*/
    Uint16 right_headphone_volume_control[2] = {0x07,0xFF};