This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教am3354从TF卡启动问题



1 第一版硬件系统能起来。

2 第二版硬件起不来,典型问题如下:七八成启动到starting Kernel 卡死不动。有个别板子可以启动到系统后半段然后卡死或者崩掉。

3 两个版本的原理图只有一个LED灯的变化。

U-Boot 2013.01.01 (Apr 19 2016 - 11:09:14)

 

I2C:   ready

DRAM:  512 MiB

WARNING: Caches not enabled

Lisa AM335x, with NO eeprom.

NAND:  No NAND device found!!!

0 MiB

MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1

*** Warning - readenv() failed, using default environment

 

musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)

musb-hdrc: MHDRC RTL version 2.0

musb-hdrc: setup fifo_mode 4

musb-hdrc: 28/31 max ep, 16384/16384 memory

USB Peripheral mode controller at 47401000 using PIO, IRQ 0

musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)

musb-hdrc: MHDRC RTL version 2.0

musb-hdrc: setup fifo_mode 4

musb-hdrc: 28/31 max ep, 16384/16384 memory

USB Host mode controller at 47401800 using PIO, IRQ 0

Net:   <ethaddr> not set. Validating first E-fuse MAC

cpsw, usb_ether

Hit any key to stop autoboot:  0

mmc0 is current device

SD/MMC found on device 0

reading uEnv.txt

** Unable to read file uEnv.txt **

reading uImage

2821400 bytes read in 297 ms (9.1 MiB/s)

Booting from mmc ...

## Booting kernel from Legacy Image at 80007fc0 ...

   Image Name:   Linux-3.2.0

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    2821336 Bytes = 2.7 MiB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... OK

   XIP Kernel Image ... OK

OK

 

Starting kernel ...