This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助DSP TMS320C5517编程中的一些名词意思



#define SYS_EXBUSSEL       *(volatile ioport Uint16*)(0x1c00)
#define SYS_PCGCR1         *(volatile ioport Uint16*)(0x1c02)
#define SYS_PCGCR2         *(volatile ioport Uint16*)(0x1c03)
#define SYS_PRCNTR         *(volatile ioport Uint16*)(0x1c04)
#define SYS_PRCNTRLR       *(volatile ioport Uint16*)(0x1c05)
#define SYS_GPIO_DIR0      *(volatile ioport Uint16*)(0x1c06)
#define SYS_GPIO_DIR1      *(volatile ioport Uint16*)(0x1c07)
#define SYS_GPIO_DATAIN0   *(volatile ioport Uint16*)(0x1c08)
#define SYS_GPIO_DATAIN1   *(volatile ioport Uint16*)(0x1c09)
#define SYS_GPIO_DATAOUT0  *(volatile ioport Uint16*)(0x1c0a)
#define SYS_GPIO_DATAOUT1  *(volatile ioport Uint16*)(0x1c0b)
#define SYS_OUTDRSTR       *(volatile ioport Uint16*)(0x1c16)
#define SYS_SPPDIR         *(volatile ioport Uint16*)(0x1c17)

/* ------------------------------------------------------------------------ *
 *  I2C Module                                                              *
 * ------------------------------------------------------------------------ */
 
#define I2C_IER            *(volatile ioport Uint16*)(0x1A04)
#define I2C_STR            *(volatile ioport Uint16*)(0x1A08)
#define I2C_CLKL           *(volatile ioport Uint16*)(0x1A0C)
#define I2C_CLKH           *(volatile ioport Uint16*)(0x1A10)
#define I2C_CNT         *(volatile ioport Uint16*)(0x1A14)
#define I2C_DRR         *(volatile ioport Uint16*)(0x1A18)
#define I2C_SAR            *(volatile ioport Uint16*)(0x1A1C)
#define I2C_DXR            *(volatile ioport Uint16*)(0x1A20)
#define I2C_MDR            *(volatile ioport Uint16*)(0x1A24)
#define I2C_EDR            *(volatile ioport Uint16*)(0x1A2C)
#define I2C_PSC            *(volatile ioport Uint16*)(0x1A30)
/* ------------------------------------------------------------------------ *
 *  I2S Module                                                              *
 * ------------------------------------------------------------------------ */
#define I2S0_CR            *(volatile ioport Uint16*)(0x2800)
#define I2S0_SRGR          *(volatile ioport Uint16*)(0x2804)
#define I2S0_W0_LSW_W      *(volatile ioport Uint16*)(0x2808)
#define I2S0_W0_MSW_W      *(volatile ioport Uint16*)(0x2809)
#define I2S0_W1_LSW_W      *(volatile ioport Uint16*)(0x280C)
#define I2S0_W1_MSW_W      *(volatile ioport Uint16*)(0x280D)
#define I2S0_IR            *(volatile ioport Uint16*)(0x2810)
#define I2S0_ICMR          *(volatile ioport Uint16*)(0x2814)
#define I2S0_W0_LSW_R      *(volatile ioport Uint16*)(0x2828)
#define I2S0_W0_MSW_R      *(volatile ioport Uint16*)(0x2829)
#define I2S0_W1_LSW_R      *(volatile ioport Uint16*)(0x282C)
#define I2S0_W1_MSW_R      *(volatile ioport Uint16*)(0x282D)
/* I2S2 */
#define I2S2_CR            *(volatile ioport Uint16*)(0x2A00)
#define I2S2_SRGR          *(volatile ioport Uint16*)(0x2A04)
#define I2S2_W0_LSW_W      *(volatile ioport Uint16*)(0x2A08)
#define I2S2_W0_MSW_W      *(volatile ioport Uint16*)(0x2A09)
#define I2S2_W1_LSW_W      *(volatile ioport Uint16*)(0x2A0C)
#define I2S2_W1_MSW_W      *(volatile ioport Uint16*)(0x2A0D)
#define I2S2_IR            *(volatile ioport Uint16*)(0x2A10)
#define I2S2_ICMR          *(volatile ioport Uint16*)(0x2A14)
#define I2S2_W0_LSW_R      *(volatile ioport Uint16*)(0x2A28)
#define I2S2_W0_MSW_R      *(volatile ioport Uint16*)(0x2A29)
#define I2S2_W1_LSW_R      *(volatile ioport Uint16*)(0x2A2C)
#define I2S2_W1_MSW_R      *(volatile ioport Uint16*)(0x2A2D)

/* ------------------------------------------------------------------------ *
 *  UART Module                                                             *
 * ------------------------------------------------------------------------ */
#define UART_RBR           *(volatile ioport Uint16*)(0x1B00)
#define UART_THR           *(volatile ioport Uint16*)(0x1B00)
#define UART_IER           *(volatile ioport Uint16*)(0x1B02)
#define UART_IIR           *(volatile ioport Uint16*)(0x1B04)
#define UART_FCR           *(volatile ioport Uint16*)(0x1B04)
#define UART_LCR           *(volatile ioport Uint16*)(0x1B06)
#define UART_MCR           *(volatile ioport Uint16*)(0x1B08)
#define UART_LSR           *(volatile ioport Uint16*)(0x1B0A)
#define UART_SCR           *(volatile ioport Uint16*)(0x1B0E)
#define UART_DLL           *(volatile ioport Uint16*)(0x1B10)
#define UART_DLH           *(volatile ioport Uint16*)(0x1B12)
#define UART_PWREMU_MGMT   *(volatile ioport Uint16*)(0x1B18)

请问这些名词都是什么意思,后面对应的地址是存储这些名词的值吗还是什么其他的