If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The CCSv3 projects files can be imported into the newer versions of Code Composer Studio, such as CCS v5.1.0. It is recommended to use the default import options when doing so. Do not copy the project files into your workspace. They should be left in place.