This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于dm365 lcd显示视频的问题续



尊敬的老师:

非常感谢您对https://www.deyisupport.com/question_answer/f/22/p/1292/3176.aspx#3176的回复。我仔细阅读了你的建议http://processors.wiki.ti.com/index.php/Adding_Display_Resolutions_to_DMAI

但是还是有一些疑问。

从文章上看虽然是dvsdk2的但我对照dvsdk4里面,应该是可以用的。

文章中的做法就是首先需要lcd的驱动(文章中是avnetlcd_encoder.c),

static struct avnetlcd_encoder_config avnetlcd_encoder_configuration = {
       .no_of_outputs = AVNETLCD_ENCODER_MAX_NO_OUTPUTS,
       .output[0] = {
                     .output_name = VID_ENC_OUTPUT_LCD1,//vid_encoder_types.h中有#define VID_ENC_OUTPUT_LCD1       "LCD1"
                     .no_of_standard = AVNETLCD_ENCODER_GRAPHICS_NUM_STD,
                     .standards[0] = {
                                      .name = VID_ENC_STD_800x480,
                                      .std = 1,
                                      .if_type = VID_ENC_IF_PRGB,
                                      .interlaced = 0,
                                      .xres = 800,
                                      .yres = 480,
                                      .fps = {60, 1},
                                      .left_margin = 216,
                                      .right_margin = 40,
                                      .upper_margin = 32,
                                      .lower_margin = 11,
                                      .hsync_len = 9,
                                      .vsync_len = 9,
                                      .flags = 0},
                     },        /* hsync -ve, vsync -ve */
};

然后在应用程序display.c中添加

/* Strings for sysfs video output variables */
static Char *outputStrings[Display_Output_COUNT] = {
   "SVIDEO",
   "COMPOSITE",
   "COMPONENT",
   "LCD",
   "LCD1", //似乎是通过“LCD1”这个名字与上面驱动中的红字部分关联起来
   "DVI",
   NULL
};
这样应用程序中便可以象普通显示设备一样使用LCD1。

但我的第一个疑问是:文章的前部分,在dmai的appMain.c添加lcd的配置信息(即Display_Attrs_DM365_OSD_DEFAULT)是干什么用的?好像这个配置和驱动程序没有什么关联的地方或语句?应用程序main.c也没有display.c那样引用"LCD1",但从Display_Attrs_DM365_OSD_DEFAULT的定义又感觉确实和LCD显示有关,真不知道这个Display_Attrs_DM365_OSD_DEFAULT是如何和驱动关联起来?

注:Display_Attrs_DM365_OSD_DEFAULT和缺省的Display_Attrs_DM365_VID_DEFAULT的区别就是:1)显示设备不同(vid是/dev/video2,osd是/dev/fb0);2)colorspace不同(vid是NV12,osd是RGB565)。

另一个问题是如上面“注”所说,Display_Attrs_DM365_OSD_DEFAULT接收的数据是RGB565,那么NV12视频数据该如何显示在LCD上呢?