This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hyperlink设计咨询

Other Parts Discussed in Thread: TMS320C6678

目前我们设计的板卡上只有一片tms320C6678,板卡采用VPX的结构,然后想将Hyperlink的接口通过后面的MultiGig RT2连接器插座引到背板上,然后通过印制板走线和其他板卡上的6678的Hyperlink接口进行通信,目前存在以下疑问:1、Hyperlink信号对接插件的指标要求是否有指定,是否只能选择开发板上使用的molex公司的接插件型号,然后能不能使用tyco公司的MultiGig RT2连接器(大概参数为:特性阻抗可控,插入损耗低,而且在传输速率达6.25Gbps时,串扰小于3%。)  2、Hyperlink的有效传递数据的PCB走线长度最长可以走多少长度呢?

望工程师解答,谢谢