各位好,
我用DM8148,基于RDK3.8,ISS采用OTF模式接收12bit 的raw图,HDMI输出显示。产品在做静电测试时,由于静电干扰,输入到DM8148的VD/HD信号也会受干扰,在严重的情况下整个图像就会卡死。 经过跟踪发现,主核A8这边能正常工作,而控制ISS的M3核程序会挂掉,这种情况有时候没有图像输出了(直接黑屏),有时候图像还会正常输出(这个时候是实时图像,但是图像出现断层,看起就是内存里的帧与帧没有同步刷新,图像一部分是上一帧一部分是下一帧)。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位好,
我用DM8148,基于RDK3.8,ISS采用OTF模式接收12bit 的raw图,HDMI输出显示。产品在做静电测试时,由于静电干扰,输入到DM8148的VD/HD信号也会受干扰,在严重的情况下整个图像就会卡死。 经过跟踪发现,主核A8这边能正常工作,而控制ISS的M3核程序会挂掉,这种情况有时候没有图像输出了(直接黑屏),有时候图像还会正常输出(这个时候是实时图像,但是图像出现断层,看起就是内存里的帧与帧没有同步刷新,图像一部分是上一帧一部分是下一帧)。
想知道VD/HD出现干扰时,ISS M3核出现卡死是不是正常现象,如果是正常现象,我能怎么在不重启系统的情况下采用软件解决这个问题?如果不是正常现象,通常需要修改哪些配置?
你好,
打静电的测试不是正常的工作情况,所以会出现什么样的情况都是可能的。
如果只是采集和显示不正常,可尝试复位ISS和HDVPSS。但是如果是M3挂起,建议复位整个芯片。