还有KeyStone II device和KeyStone I device有什么区别?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢Thomas!
后来打开了提供的链接:
TI's KeyStone II Architecture provides a programmable platform integrating various subsystems (Quad ARM Cortex-A15 CorePAc, C66x DSP CorePacs, IP network, radio layers 1, 2, and 3, and transport processing) and uses a queue-based communication system that allows the SoC resources to operate efficiently and seamlessly.
6678应该属于keystone
具体分类可以参考
http://processors.wiki.ti.com/index.php/C6000_MultiCore_Devices
TMS320C6678属于Keystone I
多核ARM+ DSP的构架属于Keystone II