This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 spi norflash启动参数问题

想请问下,在做SPI的nor下载镜像的时候,前面的DDR3 boot table:
00 00 00 70 00 87 35 00 02 42 80 F5 00 00 00 00 00 00 00 1C 00 00 00 02
63 06 2A 32 00 00 00 00 00 00 14 50 11 13 78 3C 30 71 7F E3 55 9F 86 AF
00 00 00 00 00 00 00 00 00 00 00 00 00 01 00 00 00 00 00 00 00 00 00 00
00 00 00 00 70 07 32 14 00 00 00 00 00 10 01 0F 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 10 00 00 00 00 00 00 00 00 00 00 00 00 00 03 05    这些参数是什么意思?内容可以更改吗?有什么文档是介绍这个表的呢?我随便更改一个就启动不了,但是我的DDR和开发板的DDR不一样,所以有些DDR参数是不对的。需要更改,请问应该怎么更改?

  • 可以参考processor sdk里的tiboot.h头文件里的

    * Emif4 (DDR3) configuration table

    *******************************************************************************/

    typedef struct bootEmif4Tbl_s  {

       UINT32  configSelect;               /* Bit map defining which registers to set */

       UINT32  pllPrediv;                  /* Values of all 0s will disable the pll */

       UINT32  pllMult;

       UINT32  pllPostDiv;

       UINT32  sdRamConfig;

       UINT32  sdRamConfig2;

       UINT32  sdRamRefreshCtl;

       UINT32  sdRamTiming1;

       UINT32  sdRamTiming2;

       UINT32  sdRamTiming3;

       UINT32  lpDdrNvmTiming;

       UINT32  powerManageCtl;

       UINT32  iODFTTestLogic;

       UINT32  performCountCfg;

       UINT32  performCountMstRegSel;

       UINT32  readIdleCtl;

       UINT32  sysVbusmIntEnSet;

       UINT32  sdRamOutImpdedCalCfg;

       UINT32  tempAlterCfg;

       UINT32  ddrPhyCtl1;

       UINT32  ddrPhyCtl2;

       UINT32  priClassSvceMap;

       UINT32  mstId2ClsSvce1Map;

       UINT32  mstId2ClsSvce2Map;

       UINT32  eccCtl;

       UINT32  eccRange1;

       UINT32  eccRange2;

       UINT32  rdWrtExcThresh;

    3173.tiboot_c66x.h

  • 我参考了,然后我根据这个修改了UINT32 sdRamConfig; UINT32 sdRamConfig2;就不行,只要变动1都不行,是不是这个数据结构有做校验?