1.同样一个程序在片上空间运行正常,在DDR2中运行过程中总是跑飞
2.在DDR2中运行时,DDR2的初始化配置是在GEL文件中完成的
3.开始配置DDR2的工作时钟为144MHz,时钟频率降低后程序运行时仍有跑飞现象,DDR2芯片型号为MT47H32M16-3
请教各位工程师,该现象是什么原因造成的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以看一下置顶贴里DDR压力测试例程,可以看一下DDR是否能稳定工作。
e2echina.ti.com/.../121580
DDR不稳定的话,还要检查PCB布线。