This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

仿真器连接上DSP6701后程序无法加载

DSP6701连接问题

我连的过程中CCS5.5及8.0两个版本都用过,连接DSP按正常流程,先LAUNCH找到仿真器,后连接DSP,连接后初始值为0x0000000,认定已经连接上了DSP。在此情况下,去读DSP的内部RAM,同时也可以修改RAM值 ,下电再上电后,修改的RAM值也可以被擦除。但后续load程序,想在线运行时,程序直接就跑飞,按了暂停键后,界面提示“设备未响应请求,重置设备并重新操作。如果持续错误,确认配置,硬件外围等."   示波器测试DSP的复位、晶振、电源都正常。两个CLKOUT的输出频率也都对,现在不知道问题出在哪里,求帮助,谢谢大家。