XDS200, CCS5.3安装后,插上仿真器,设备管理器里只能找到两个串行端口,其中一上有问号。另一个正常。没有其他XDS200 仿真器设备。在 CCS5.3中配置好目标板,运行时显示-2083. 显示无法初始化仿真器。但在TI的网站和SD的网站上,都无法找到另外的关于XDS200的驱动。且因为较新,也没有更多的参考。现一直无法使用,请帮忙诊断。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
XDS200, CCS5.3安装后,插上仿真器,设备管理器里只能找到两个串行端口,其中一上有问号。另一个正常。没有其他XDS200 仿真器设备。在 CCS5.3中配置好目标板,运行时显示-2083. 显示无法初始化仿真器。但在TI的网站和SD的网站上,都无法找到另外的关于XDS200的驱动。且因为较新,也没有更多的参考。现一直无法使用,请帮忙诊断。
你的目标板是什么DSP? XDS200不支持一些老的DSP.
http://processors.wiki.ti.com/index.php/Xds200#Q:_What_devices_are_supported_by_XDS2xx.3F
谢谢回复。我的操作系统是32位XP。目标芯片为28035或6446.。故障现象均一样。运行test connection时,显示如下信息。就和没接仿真器一样。我现在需要确定的是,CCS5.3是不是自带USB端的XDS200的驱动?安装后CCS5.3后,不需要再另外给XDS200安装驱动了吗?如果安装成功,设备管理器的名称叫什么?我现在中能找到两个串口。如附图
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -r -o -S pathlength -S integrity
[Result]
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_io
Failed to open i/o connection (xds2xxu:0)
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the named emulator via USCIF ECOM has failed.
[End]
ccs v5.3以上的版本自带xds200仿真器驱动, 不需要额外安装. 你的设备管理器名字是对的, 试试按照下面的步骤更新一下驱动, 目前最新的是5.0.899.0.